EAGLE User Support (English) Possible Eagle ltspice.ulp redundancy "SPICEMODEL" attribute
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 552 views
  • Users 0 members are here
  • ltspice
  • modelfile
  • spicemodel
  • ltspiceiv
Related

Possible Eagle ltspice.ulp redundancy "SPICEMODEL" attribute

svangool
svangool over 9 years ago

I think there is a misconception in the Eagle ltspice.ulp about the use of "SpiceModel":

 

Within LTSpiceIV (no effect within Eagle) the "ModelFile" indicates a library of one or more sub-circuits/models within one file, the "ModelFile" requires a filename with syntax [<folder>/]<name>[.<ext>] within the standard  \lib\sub\ folder, normally containing the standard sub-circuits/models.

If you want to change, during simulation in LTSpice, the model of a library device, e.g. another voltage for a TVS from the SMAJxxx_CA library, the "SpiceModel" field defines the default model and lets you select one of sub-circuits/models defined in the library from a drop-down list if you click it, if the "ModelFile" exists. The "SpiceModel" field should then contain a valid sub-circuit/model-name from the library file or be empty.

 

In the Eagle ltspice.ulp, "ModelFile" field is not generated, there is no means of defining the filename for auto symbol generation from the attributes.

Therefor, I think, it makes no sense that "SpiceModel" is implemented, because the "ModelFile" (assuming that the symbols for libraries are auto-generated) is never there.

In the current state it only makes sense to not define the attribute or put "NONE" in the "SpiceModel" field (which the ltspice.ulp skips) of the symbol export, it is only a nuisance now because there is no additional value for defining "SpiceModel".

There can be value for defining the "SpiceModel" field, if a "ModelFile" attribute would also be processed by the ltspice.ulp.


Maybe I missed another usage for the "ModelFile" generation by the ltspice.ulp, then I would be glad to learn its usage.


Best regards, Sjef.

  • Sign in to reply
  • Cancel

Top Replies

  • svangool
    svangool over 9 years ago in reply to clem57 +1
    I don't think so, It wouldn't make a lot of sense and it is hindering. I hope someone of Cadsoft can shed some light (Jorge?).
  • clem57
    0 clem57 over 9 years ago

    Eagle is known to add things for future enhancements. This may be one o those.image

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • svangool
    0 svangool over 9 years ago in reply to clem57

    I don't think so, It wouldn't make a lot of sense and it is hindering. I hope someone of Cadsoft can shed some light (Jorge?).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to svangool

    On 1/25/2016 3:56 AM, Sjef van Gool wrote:

    I don't think so, It wouldn't make a lot of sense and it is hindering. I

    hope someone of Cadsoft can shed some light (Jorge?).

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/172602

     

    Hi Sjef,

     

    Unfortunately, I haven't dedicated enough time to that ULP to be able to

    really know if it's redundant or not. I've been wanting to get into that

    ULP for some time, but my daily support work has not permitted it.

     

    The original author of the ULP is not available for comment, I'm really

    going to have to make some time for this soon.

     

    I wish I had better news.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to svangool

    On 1/25/2016 3:56 AM, Sjef van Gool wrote:

    I don't think so, It wouldn't make a lot of sense and it is hindering. I

    hope someone of Cadsoft can shed some light (Jorge?).

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/172602

     

    Hi Sjef,

     

    Unfortunately, I haven't dedicated enough time to that ULP to be able to

    really know if it's redundant or not. I've been wanting to get into that

    ULP for some time, but my daily support work has not permitted it.

     

    The original author of the ULP is not available for comment, I'm really

    going to have to make some time for this soon.

     

    I wish I had better news.

     

    Best Regards,

    Jorge Garcia