EAGLE User Support (English) MOVING SMD PADS
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 1065 views
  • Users 0 members are here
Related

MOVING SMD PADS

Former Member
Former Member over 10 years ago

I'm new at Eagle and I am trying to make my first SMD footprint. I have the grid set at 1 mm alt at .05.  When I try to put the first pad at 0,1.2 I find that the displayed coordinates are relative to where the CURSOR is in the pad, not the pad itself. I seems like I need one of two things to position the pads accurately: 1: be able to select the pad at dead center or 2: be able to let the coordinates reflect the center of the pad instead of the cursor position.

 

I guess my question to the community is, how do you place pads accurately in Eagle 7.5?

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago +1 verified
    On 31/01/2016 3:10 p.m., Picky Biker wrote: I'm new at Eagle and I am trying to make my first SMD footprint. I have the grid set at 1 mm alt at .05. When I try to put the first pad at 0,1.2 I find that…
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 31/01/2016 3:10 p.m., Picky Biker wrote:

    I'm new at Eagle and I am trying to make my first SMD footprint. I have

    the grid set at 1 mm alt at .05.  When I try to put the first pad at

    0,1.2 I find that the displayed coordinates are relative to where the

    CURSOR is in the pad, not the pad itself. I seems like I need one of two

    things to position the pads accurately: 1: be able to select the pad at

    dead center or 2: be able to let the coordinates reflect the center of

    the pad instead of the cursor position.

     

    I guess my question to the community is, how do you place pads

    accurately in Eagle 7.5?

     

     

    When placing an SMD in the package editor, the pad will try to snap to

    the grid point closest to the cursor.

     

    To place the smd at a specific place, ignoring the grid, simply enter

    the coordinates into the command line.

     

    For your case you would select the smd icon and then with the smd

    foating with the cursor enter into the into the command line (0 1.2)

    . The smd will be placed with its origin at  x=0 y=1.2mm. After

    that you can rotate and change its size if they have not been set up

    before hand.

     

    All that entering into the command line is a pain when there are many

    pads to do that are spaced horizontally or vertically with regular

    spacing so you can use the grid to do the hard work and avoid the maths.

     

    We let Eagle do the hard work for us and use a feature of the grid.

    No matter where an object is, if you change the grid and copy or move

    the object it will step the distance of the new grid. Its like an

    invisible grid belonging only to that object.

     

    Lets say an imaginary component needs a horizontal row of six pads

    1.73mm apart and above the origin 1.57mm and symmetrically left and

    right of the origin You will have detected that the maths will be doable

    but repetitious.

     

    The method works as follows:

    Set the grid to 1.57mm

    Place a smd at x=0 y=1.57 which is easily done as there is a grid to

    snap it to. No need to use the command line and it sits at the correct

    height above the origin.

     

    Change the grid to 0.865mm (half our 1.73mm spacing) this is our only maths.

    Move the smd one step left.

    Change the grid to 1.73mm

    Move the smd two steps left (This is the left most smd we need)

    Copy this smd to the right five times to attain the needed row of six

    smd spaced at 1.73mm

     

    job done

     

    HTH

    Warren

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 31/01/2016 3:10 p.m., Picky Biker wrote:

    I'm new at Eagle and I am trying to make my first SMD footprint. I have

    the grid set at 1 mm alt at .05.  When I try to put the first pad at

    0,1.2 I find that the displayed coordinates are relative to where the

    CURSOR is in the pad, not the pad itself. I seems like I need one of two

    things to position the pads accurately: 1: be able to select the pad at

    dead center or 2: be able to let the coordinates reflect the center of

    the pad instead of the cursor position.

     

    I guess my question to the community is, how do you place pads

    accurately in Eagle 7.5?

     

     

    When placing an SMD in the package editor, the pad will try to snap to

    the grid point closest to the cursor.

     

    To place the smd at a specific place, ignoring the grid, simply enter

    the coordinates into the command line.

     

    For your case you would select the smd icon and then with the smd

    foating with the cursor enter into the into the command line (0 1.2)

    . The smd will be placed with its origin at  x=0 y=1.2mm. After

    that you can rotate and change its size if they have not been set up

    before hand.

     

    All that entering into the command line is a pain when there are many

    pads to do that are spaced horizontally or vertically with regular

    spacing so you can use the grid to do the hard work and avoid the maths.

     

    We let Eagle do the hard work for us and use a feature of the grid.

    No matter where an object is, if you change the grid and copy or move

    the object it will step the distance of the new grid. Its like an

    invisible grid belonging only to that object.

     

    Lets say an imaginary component needs a horizontal row of six pads

    1.73mm apart and above the origin 1.57mm and symmetrically left and

    right of the origin You will have detected that the maths will be doable

    but repetitious.

     

    The method works as follows:

    Set the grid to 1.57mm

    Place a smd at x=0 y=1.57 which is easily done as there is a grid to

    snap it to. No need to use the command line and it sits at the correct

    height above the origin.

     

    Change the grid to 0.865mm (half our 1.73mm spacing) this is our only maths.

    Move the smd one step left.

    Change the grid to 1.73mm

    Move the smd two steps left (This is the left most smd we need)

    Copy this smd to the right five times to attain the needed row of six

    smd spaced at 1.73mm

     

    job done

     

    HTH

    Warren

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer