Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Tidy schematic after pinswap
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 191 subscribers
  • Views 2455 views
  • Users 0 members are here
  • pinswap schematic
Related

Tidy schematic after pinswap

alberthall
alberthall over 10 years ago

I am working on a design using a microcontroller using analogue inputs and digital I/O.   The analogue pins can be swapped and the digital pins can be swapped at will (with commensurate changes in the firmware).  I have set the swap levels on the part to allow this.  I put short wires on each pin and named them and did likewise with the parts they connected to.  The parts on the board layout are connected correctly but the layout would be better if some pins were swapped.   So, on the schematic I swap some pins and the board layout correctly reflects the changes.   The problem is that the schematic is now a mess wire wires draped all over the microcontroller.  I tried using Bus/Net but the result is similar.

 

Is there a way of using pinswap without making a mess of the schematic?

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    Olin Lathrop wrote:

     

    James Thurgood wrote on Sat, 06 February 2016 09:07

    Is there a way of using pinswap without making a mess of the schematic?

     

    Stop and actually think about it.  How do you expect this to work?  Laying

    out a schematic to be nicely readable requires much higher level judgement

    above the mere connection topology Eagle knows about.

     

    Why? To swap two equivalent pins on the board you only have to change the

    pin number in the schematic, nothing has to be redrawn (otherwise the pins

    were not swapable in the first place).

     

    Gruss, Matthias Dingeldein

     

    --

    Guillotinen sind nicht reziprok, aber das macht nix,

    die werden eh nur fuer die Hinrichtung verwendet

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    James Thurgood wrote on Sat, 06 February 2016 09:07

    Is there a way of using pinswap without making a mess of the schematic?

     

     

    Stop and actually think about it.  How do you expect this to work?  Laying

    out a schematic to be nicely readable requires much higher level judgement

    above the mere connection topology Eagle knows about.  This isn't going to

    work for the same reason Eagle doesn't have some automatic "beautify"

    function for the schematic.  Too much high level knowledge and artistic

    judgement is required to do anything useful, not to mention the algorithms

    would be very complex even if this were possible somehow.

     

    It will continue to be your job to draw a clear schematic for the

    reasonably forseable future.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
<