Hi,
I'm trying to make my own Device,
I have created the symbol and the package, when trying to connect the symbol to the package I don't see the names of the pins eventhough I named them carefully (as shown in the picture below)
any Idea, thanks
Hi,
I'm trying to make my own Device,
I have created the symbol and the package, when trying to connect the symbol to the package I don't see the names of the pins eventhough I named them carefully (as shown in the picture below)
any Idea, thanks
that was a silly mistake,
Thank you so much
In the library editor click on the device button and select your device
from the list and open it.
You'll now see a window with three areas. The top left is the area which
will show any added symbols, below that shows any description and any
device attributes and to the right is where you specify packages and
variants.
On the left hand side there is a tool bar and on there you will find the
add button. In Eagle 7.x it looks like an AND gate with a + symbol on top
and a downwards black arrow. Click on that. You'll now see a list of all
the symbols in your library. Select your symbol for this part and click OK.
You will then be prompted to place it down in the top left area much like
when you place a symbol on a schematic.
Once you have done this the pin names should appear in your list for
assigning footprint pins to them.
There are some really good tutorials on the internet showing you the basics
of building your own library parts. Try these two as a starting point:
http://dangerousprototypes.com/2012/03/07/how-to-make-parts-in-cadsoft-eagle/
https://learn.adafruit.com/eagle-tutorial-how-to-add-a-new-package-to-a-component/
Hope this helps,
Rachael
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
@rachaelp : How do I add the symbol to the part?
Mohamed Amini wrote on Tue, 09 February 2016 11:26
Hi,
I'm trying to make my own Device,
I have created the symbol and the package, when trying to connect the
symbol to the package I don't see the names of the pins eventhough I
named them carefully (as shown in the picture below)
any Idea, thanks
--
To view any images and attachments in this post, visit:
You have to set the "visible" parameter for each pin.
From the help for the pin command...
Quote:
Visible
This parameter defines if pin and/or pad name are visible in the
schematic:
Off
pin and pad name not drawn
Pad
pad name drawn, pin name not drawn
Pin
pin name drawn, pad name not drawn
Both
pin and pad name drawn
Default: Both
To do a group change:
Select the group command Click and drag a rectangle OR multi-click a
polygon around all of the pins Type "change visible both" --where both is
the value you want to see both pin number and pad name Apply the command to
the group. By default this is CTRL/CMD and right-click (I prefer the old
right-click that you can get back by using the SET command)
James,
--
James Morrison ~~~ Stratford Digital
Order your EAGLE license from Stratford Digital at
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
When you created the part, did you add the symbol to the part? It looks
like you possibly didn't. Alternatively how did you create the pins on the
symbol? More pictures or the library adding here would be helpful.
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.