Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Op Amp symbol as triangle, not rectangle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 189 subscribers
  • Views 2501 views
  • Users 0 members are here
Related

Op Amp symbol as triangle, not rectangle

r_iot
r_iot over 10 years ago

Hi,

 

New to Eagle.

I'm using a Microchip dual op amp MCP6002 in my schematic.

I've successfully downloaded the Microchip library however the IC displays as a single block rectangle and not as two individual (triangles) op amps. This doesn't make for easy schematic viewing so wondering if there's a way to convert MCP6002 symbol into two individual op amps, each with triangle symbol but together using the same pad layout (with different pins of course). Very happy to look at any tutorials/docs if anyone can point me in the right direction. Thanks.

 

kind regards,

 

Stuart

  • Sign in to reply
  • Cancel
  • r_iot
    0 r_iot over 10 years ago in reply to autodeskguest

    Hi all,

     

    Many thanks for the excellent feedback.

    I'm working my way through the tutorials as mentioned in Rachel's post.

     

    I'll adopt strategy as per Warren's post and use the AD or Linear part as mentioned earlier:

    "learn how to copy that whole device across to your personal

    library and change its name , description, attributes until its what you

    want"

     

    cheers,

     

    Stuart

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago

    As has been said, most downloaded library parts are really poor quality and

    I agree the rectangular box op-amps with it all in one package are really

    annoying and as you say, don't make for readable schematics.

     

    Here are a couple of good tutorials you can go through to get the

    essentials of what you need to do, although they do also just use

    rectangular symbols with names in pin order so don't take them too

    literally, just use the techniques shown:

     

    From Adafruit:

    https://learn.adafruit.com/ktowns-ultimate-creating-parts-in-eagle-tutorial/introduction

    From Dangerous Prototypes:

    http://dangerousprototypes.com/docs/Cadsoft_Eagle_how_to_make_parts_tutorial

     

    Once you get the hang of the basics you can then build on that with more

    advanced features like technologies, variants and enabling pin swapping

    etc.

     

    Here is a site with a few tutorials on these topics:

    http://blog.ilektronx.com/search/label/eagle%20tutorial

     

    Best Regards,

     

    Rachael

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 26/02/2016 6:34 a.m., Stuart Robertson wrote:

    Hi,

     

    New to Eagle.

    I'm using a Microchip dual op amp MCP6002 in my schematic.

    I've successfully downloaded the Microchip library however the IC

    displays as a single block rectangle and not as two individual

    (triangles) op amps. This doesn't make for easy schematic viewing so

    wondering if there's a way to convert MCP6002 symbol into two individual

    op amps, each with triangle symbol but together using the same pad

    layout (with different pins of course). Very happy to look at any

    tutorials/docs if anyone can point me in the right direction. Thanks.

     

    Hi

    There are many tutorials out there. I would recommend watching a couple

    of videos to quickly reach an understanding of how 'Packages', 'Symbols'

    come together to make a 'Device'.

     

     

    One thing for sure is that to use Eagle you will need to learn how to

    make library components. So settle in and do tutorials

     

    The Eagle manual (Chapter 8) explains it well. The manual is in the

    Documentation Folder in the Control Panel.

     

    Fortunately there is already a device in the Eagle provided libraries

    that seems to be a copy of your needs.

     

    AD712

    analog-devices.lbr

     

    If so, learn how to copy that whole device across to your personal

    library and change its name , description, attributes until its what you

    want. You can practice using it on a dummy schematic. When you ADD that

    AD712 to the schematic it delivers both OP amps and the power pins in

    one go. Compare that with a 7400 device where the gates are added one at

      a time and you INVOKE on a placed gate to select the power pins to place.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to autodeskguest

    Hi Stuart,

     

    Also, Rob has a good point, since your part has a normal op amp topology, you could use one of the other correctly drawn op amps that are part of the default libraries in EAGLE.

    Once you place it on your schematic, you can click on the 'Value' icon in the toolbar, select the op amp and rename it to MCP6002.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • r_iot
    0 r_iot over 10 years ago in reply to autodeskguest

    Hi,

     

    Thanks !

    I'll look to use the Linear part as a template and start to create my own library.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • r_iot
    0 r_iot over 10 years ago in reply to shabaz

    Hi Shabaz,

     

    Thanks for the prompt feedback.

    All makes sense to me and I'll give it a go !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 25/02/16 17:34, Stuart Robertson wrote:

    Hi,

     

    New to Eagle.

    I'm using a Microchip dual op amp MCP6002 in my schematic.

    I've successfully downloaded the Microchip library however the IC

    displays as a single block rectangle and not as two individual

    (triangles) op amps. This doesn't make for easy schematic viewing so

    wondering if there's a way to convert MCP6002 symbol into two individual

    op amps, each with triangle symbol but together using the same pad

    layout (with different pins of course). Very happy to look at any

    tutorials/docs if anyone can point me in the right direction. Thanks.

     

    Sadly an awful lot of the downloadable library parts are very poorly

    implemented, as you have found. The usual advice, in fact, is never to

    trust a library you have downloaded. It's nearly always quicker to

    create your own than to carefully check and then rectify somebody else's.

     

    In this particular case, if you're using the DIL or SO-8 package, the

    MCP6002 is a perfectly ordinary, standard dual op-amp with the same

    pin-out as the "2AMP_P8+4" component in the "linear" library that is

    shipped with Eagle. I'd just use that.

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago

    Hi Stuart,

     

    Take a look at some of the op amps supplied in the default libraries with EAGLE for some ideas - they have achieved what you're asking for. Basically the trick is, they create multiple 'symbols' in a library, and then they are all applied in the 'device' view in the library.

    Google should reveal tutorials on part creation in a library (the step to apply multiple symbols is the same as the step to apply one symbol to the device, just repeat it). The EAGLE user manual is also pretty good.

    You can edit a library, but a better method is just create your own library and create parts in it as and when required. You can also copy and paste parts from one library into another if you want to, and copy and paste symbols or packages too. A lot of flexibility, the only real way to learn it is to try to create some parts just for practice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer