Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Wrong XREF coordinate.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 379 views
  • Users 0 members are here
Related

Wrong XREF coordinate.

kikoun
kikoun over 10 years ago

Hello,

 

I have some troubles with the coordinates (column/row) automatically added in net XREF label.

Every thing works fine (ie coordinates of the next XREF label are OK) if I directly draw the frame (FRAME command) in schematic.

 

But since I don't want to manually draw the FRAME each time I add a page, I create a device in my own library in witch there is a symbol with a FRAME in it (and some other stuff). When I add a new page, I add this device in it. But then all the coordinates in all the XREF are wrong (only the page number is OK).

If I remove this device, since there is no more frame, then the coordinates are replaced by '??'. This mean that Eagle detect correctly if there is a FRAME or not in that device. But it does not process the coordinate correctly because if I place again the device, coordinates appears instead of the ?? but they are wrong.

 

Now, if I draw a new FRAME in the schematic, at the exact position of the frame of the device (the 2 FRAMEs, the one of the schematic and the one from the device, are exactly at the same position, have same parameters, and have the same size), then coordinate are correct !

 

In library I tried to change the layer of the FRAME, the prefix is FRAME... I don't really know how to solve this !

Anyone have an idea ?

 

 

By the way, 2 little enhancements would be nice :

* possibility to have ALL the pages and not only the next page.

* XREF label for buses... of course!

 

Guillaume.

  • Sign in to reply
  • Cancel
  • kikoun
    0 kikoun over 10 years ago

    Hello,

     

    It seems that I'm the only one to have this problem...

    I'm sure I'm doing something wrong, but i can not figure what.

    Nobody have any tips ?

     

    Guillaume.