Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Custom device doesn't update after package editing
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 3079 views
  • Users 0 members are here
  • frontpage
Related

Custom device doesn't update after package editing

e14 Contributor
e14 Contributor over 10 years ago

Hey there,

 

I'm quite new to Eagle, so please don't throw rocks if I'm asking something basic.

I've created a custom device and after turning it into a real PCB I realized I need to modify some pads. I looked up the specific package in my library and performed the necessary changes. The problem is now that I can't get Eagle to allow me to use my updated device.

 

I am attaching a few pics to illustrate the problem:

- SPDT_device_library.png shows the device in my library. I have intentionally edited the pads on the sides to be asymmetrical, so that it would be easy to spot whether the device is updated or not

- Control panel view.png - back to my control panel, when I look inside the library, the old package is being displayed to me

- Using the device.png - not surprisingly, if I use the device in a new project, I get the old package with symmetrical side pads.

 

I can't find an explanation for what is happening here. It looks like there exists no instance of the old package. Yet somehow the device from my library is pooling out from somewhere and using the old package.

 

Your help is greatly appreciated,

Mihaela

Attachments:
image
image
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Hi

     

    If you have made the change in the library and saved it.

    Then in the board you performed a library update or update all

    and the problem persists.

    Or if you ADD the part and it is the unmodified one, then I strongly

    suspect the following:

     

    You are accessing a similarly named library in your environment.

    You could confirm another library of the same name exists by searching for

    eeg_parts.lbr

     

    There is a few reason you can target the other file.

    In Control Panel > Options > Directories > Libraries

    if there are multiple paths to library folders, they are checked left to

    right so if you library name is found in another folder, and the device

    name matches, that's the one that gets used.

     

    Another way, if you use projects, comes from your eagle.epf file in the

    project folder. There is one of these files for each project. In it there

    are paths to used library files and hence if a project came from different

    instance of Eagle it could point to the other library location. You can

    un-use all libraries by entering into the command line

    USE -*

    That will un-use all the libraries. Then you should 'use' the ones you want

    again.

     

    HTH

    Warren

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    Hi

     

    If you have made the change in the library and saved it.

    Then in the board you performed a library update or update all

    and the problem persists.

    Or if you ADD the part and it is the unmodified one, then I strongly

    suspect the following:

     

    You are accessing a similarly named library in your environment.

    You could confirm another library of the same name exists by searching for

    eeg_parts.lbr

     

    There is a few reason you can target the other file.

    In Control Panel > Options > Directories > Libraries

    if there are multiple paths to library folders, they are checked left to

    right so if you library name is found in another folder, and the device

    name matches, that's the one that gets used.

     

    Another way, if you use projects, comes from your eagle.epf file in the

    project folder. There is one of these files for each project. In it there

    are paths to used library files and hence if a project came from different

    instance of Eagle it could point to the other library location. You can

    un-use all libraries by entering into the command line

    USE -*

    That will un-use all the libraries. Then you should 'use' the ones you want

    again.

     

    HTH

    Warren

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer