Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How good is LT Spice with Eagle?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 189 subscribers
  • Views 3188 views
  • Users 0 members are here
Related

How good is LT Spice with Eagle?

matelot
matelot over 10 years ago

I am just discovering Eagle and see a box on the schematic page for LT Spice. Is it fairly straight forward to run the two together and would people recommend using both together?

thanks.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 4/14/2016 6:55 PM, matelot m wrote:

    I am just discovering Eagle and see a box on the schematic page for LT

    Spice. Is it fairly straight forward to run the two together and would

    people recommend using both together?

    thanks.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/194771

     

    Hi Matelot,

     

    Getting them to work together requires some setup that isn't entirely

    intuitive, however once everything is setup properly then they work well

    together.

     

    See this youtube video for more info:

    https://www.youtube.com/watch?v=PBEHUw7BhTs

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • matelot
    0 matelot over 9 years ago in reply to autodeskguest

    Hi Jorge,

    thanks for replying.

    The reason I have taken so long to reply is that I have spent many fruitless hours trying to get them to work together. I finally gave up and left it.

    I have recently been sent an advert saying the change of Cadsofts position makes Eagle an even better program, !sic.

    I decided to try again.

    I looked at the video you recommended and after the first 10 minutes of advert about cadsoft and eagle I got to trying to make it work with ltspice, it doesn't even tell you how to get it working it just shows you how to manipulate the two when they are working.

    For instance the first thing it says is

    click on the lt spice box and click on 'export setup' you get another box......etc

    I don't , I get  ltspiceIV (scad3.exe) not found. As I did with the lt spice I had installed then and the uptodate ltspice I have just installed. I was told to update as the lt spice IV is no longer supported. I now have lt spice xv11. The is no scad3.exe anywhere on my computer but I can run lt spice.

    I am a little concerned that when I do get it working lt spice will not accept the components that I am getting from eagle but I bet I am a long way from that.

    Bob.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to matelot

    Hi Bob,

     

    Don't use the latest LTSpice version XVII or whatever. Use LTSpice IV,

    the current ULP isn't aware of the new one so it just halts and catches

    fire.

     

    There's an effort going on right now to update the ULP to work

    cross-platform and we hope to also include support for the latest

    version of LTSpice.

     

    You can follow along at our git repo:

    https://github.com/cadsoftcomputer/EAGLE-LTSpice-port-to-Linux-and-Mac

     

    Full disclosure: I'm the one working on this.

     

    You do have to watch the whole video, I know it's long, but if you get

    far enough into it you'll see how you can address the requirement of

    correspondence between the two pieces of software.

     

    hth,

    Jorge Garcia

    Autodesk Support

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to matelot

    On 10/27/2016 6:01 PM, matelot m wrote:

    Yes, sorry I have that now.

     

    Before I go any further, I have only seen simulations of oscilloscope traces showing circuits running, is it possible to add things such as switches and be able to switch them on screen and see the effects?

    You can simulate switches, but it's not interactive. You can setup a

    delay for the switch to flip and then observe how the circuit works.

     

    I have set up my directories and the program sees lt-supply.lbr. It also shows all the libraries in the control panel  libraries/ltspice.

    I was able to load the diagram he loaded.

    This is good, that means the bridge is working.

     

    I did watch though the rest of the video but it didn't help any more.

    After I got the libraries working I watched again from 17.15 right up to 19.15 where he says he has to open a library and goes to one he has made earlier

    , ltdemo.lbr. He goes to it and suddenly there is a library editor on the screen? How did he get there?

    File > New > Library or File > Open > Library in the control. In the

    schematic or board editor you would click Library > Open.

     

    One thing I have discovered, it looks as if I will be better to abandon all the diagrams I have made up to now and remake them with lt-spice components.

    I tried to export one of my designs and the first component it found it failed as not being lt-spice compatible.

     

    No, further on in the video you'll see how to make your parts compatible

    with LTSpice.

     

    I watched the rest of the video again hoping to find how to get to the library editor and reached 20.30.

     

    At 2030 he says he had to "go find a spice model, eagle contains no spice models so I had to go find one, in my case I used the one from TI which is this one right here"  ?

    Right where?

    He doesn’t explain where they are or how to find them,  I did a search of my computer and found no *.mod files. again I am stopped and can’t continue.

    Your computer doesn't contain model files. The model files have to be

    obtained from manufacturer websites. Look at the parts you want to use,

    visit the manufacturers website and search for " spice model".

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to matelot

    On 10/27/2016 6:01 PM, matelot m wrote:

    Yes, sorry I have that now.

     

    Before I go any further, I have only seen simulations of oscilloscope traces showing circuits running, is it possible to add things such as switches and be able to switch them on screen and see the effects?

    You can simulate switches, but it's not interactive. You can setup a

    delay for the switch to flip and then observe how the circuit works.

     

    I have set up my directories and the program sees lt-supply.lbr. It also shows all the libraries in the control panel  libraries/ltspice.

    I was able to load the diagram he loaded.

    This is good, that means the bridge is working.

     

    I did watch though the rest of the video but it didn't help any more.

    After I got the libraries working I watched again from 17.15 right up to 19.15 where he says he has to open a library and goes to one he has made earlier

    , ltdemo.lbr. He goes to it and suddenly there is a library editor on the screen? How did he get there?

    File > New > Library or File > Open > Library in the control. In the

    schematic or board editor you would click Library > Open.

     

    One thing I have discovered, it looks as if I will be better to abandon all the diagrams I have made up to now and remake them with lt-spice components.

    I tried to export one of my designs and the first component it found it failed as not being lt-spice compatible.

     

    No, further on in the video you'll see how to make your parts compatible

    with LTSpice.

     

    I watched the rest of the video again hoping to find how to get to the library editor and reached 20.30.

     

    At 2030 he says he had to "go find a spice model, eagle contains no spice models so I had to go find one, in my case I used the one from TI which is this one right here"  ?

    Right where?

    He doesn’t explain where they are or how to find them,  I did a search of my computer and found no *.mod files. again I am stopped and can’t continue.

    Your computer doesn't contain model files. The model files have to be

    obtained from manufacturer websites. Look at the parts you want to use,

    visit the manufacturers website and search for " spice model".

     

    hth,

    Jorge Garcia