Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Restrict/Delete Copper pour
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 188 subscribers
  • Views 2878 views
  • Users 0 members are here
Related

Restrict/Delete Copper pour

anishkgt
anishkgt over 10 years ago

Hi All,

 

how do we restrict copper pour on some areas like when drawing a polygon no copper should be poured in that polygon.

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 10 years ago

    Hi George,

     

    You can create a polygon within another polygon and in it's properties set Polygon Pour to "cutout".

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to rachaelp

    thanks i remembering asking it earlier too but i noticed that the doted lines of the polygon appear when i try to take print for etching. so i thought there could be a better of doing it. Like the tRestrict, that was not meant of it i guess.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    thanks i remembering asking it earlier too but i noticed that the doted lines of the polygon appear when i try to take print for etching. so i thought there could be a better of doing it. Like the tRestrict, that was not meant of it i guess.

    Are you trying to print directly out of EAGLE for etching? If so I wouldn't do that, especially if it is giving you dotted lines on your cutouts! Use the CAM processor and export to gerber files and then open them using gerbv. You can then print them from there instead or export them to a different format if needed.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    thanks i remembering asking it earlier too but i noticed that the doted lines of the polygon appear when i try to take print for etching. so i thought there could be a better of doing it. Like the tRestrict, that was not meant of it i guess.

    Are you trying to print directly out of EAGLE for etching? If so I wouldn't do that, especially if it is giving you dotted lines on your cutouts! Use the CAM processor and export to gerber files and then open them using gerbv. You can then print them from there instead or export them to a different format if needed.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 9/29/2016 8:43 AM, George Thomas wrote:

    Hmmm CAM processor, well not sure how it works. I print from eagle to a transfer sheet  (http://www.ebay.com/itm/131749981665?_trksid=p2057872.m2749.l2649&ssPageName=STRK%3AMEBIDX%3AIT)and use an iron to transfer the toner to the copper board. It worked earlier.

     

    Talking about boards, does the thickness of copper on the board matter here probably not for the dc side but am concerned about the AC ? how much are available ? i got one of these (http://www.ebay.com/itm/131382284869?_trksid=p2057872.m2749.l2649&ssPageName=STRK%3AMEBIDX%3AIT). would this be ok ?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/206572

     

    Hello George,

     

    I hope you're doing well. If you're going to be doing toner transfer

    then you can use the cam2image.ulp to get high resolution images of your

    board which will work better for the transfer sheet.

     

    That ULP uses the CAM processor jobs to define what layers should be

    included in what images. Go for the highest resolution you can to get to

    most toner on the sheet.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    Hmmm CAM processor, well not sure how it works. I print from eagle to a transfer sheet and use an iron to transfer the toner to the copper board. It worked earlier.

    It's easy to use the CAM processor:

     

    Click on the CAM processor button

    Go to File->Open->Job...

    Navigate to the CAM folder and choose an appropriate file e.g. gerb274x.cam

    As you have a single layer board and you are etching it yourself just select the "Component Side" tab which will select layers 1 Top, 17 Pads and 18 Vias and the click "Process Section"

     

    Now open the resulting file in gerbv and check that it includes all you expect, then you should be able to print it out or export it for use elsewhere.

     

    George Thomas wrote:

     

    Talking about boards, does the thickness of copper on the board matter here probably not for the dc side but am concerned about the AC ? how much are available ? i got one of these. would this be ok ?

    I don't know about these copper clad boards for etching I'm afraid, I haven't etched a board since the 1990's as prototype PCB's are so cheap to get made now. If I was having a PCB made that had either high current or a lot of heat generated then I would go for a board with heavier copper. The board you link to gives just the overall board thickness but no info on the weight of copper so I don't know how it compares to purchased PCB's.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to rachaelp

    Hmmm CAM processor, well not sure how it works. I print from eagle to a transfer sheet and use an iron to transfer the toner to the copper board. It worked earlier.

     

    Talking about boards, does the thickness of copper on the board matter here probably not for the dc side but am concerned about the AC ? how much are available ? i got one of these. would this be ok ?