Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How do I control pad to polygon connection?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 2116 views
  • Users 0 members are here
  • mask
  • pad
  • polygon
Related

How do I control pad to polygon connection?

arbutus
arbutus over 10 years ago

Perhaps I'm missing something, but now (using Eagle 7.6.0) any pads matching the polygon signal are connected by hair-thin traces, not by the solid pour I would expect.

 

contentimage_75913.tiff

For example on R4 I would expect to see no isolation between the through-hole part (lower pin) and the Layer 16 (GND) polygon. 

The designs pass ERC/DRC - is there a parameter in the autorouter setup I can adjust to cure this?

 

What controls this behaviour?

 

Thanks for any advice!

  • Sign in to reply
  • Cancel
Parents
  • arbutus
    0 arbutus over 10 years ago

    Ok so the resolution was the boundary thickness (line width) of the polygon, combined with the ISOLATE parameter. 

     

    It seems strange that there is no granular control of this style - the size of the pad and the polygon boundary should be related otherwise large pads and small pads on the same polygon behave very differently.

     

    Thanks for the help !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • arbutus
    0 arbutus over 10 years ago

    Ok so the resolution was the boundary thickness (line width) of the polygon, combined with the ISOLATE parameter. 

     

    It seems strange that there is no granular control of this style - the size of the pad and the polygon boundary should be related otherwise large pads and small pads on the same polygon behave very differently.

     

    Thanks for the help !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to arbutus

    Don Gibson schrieb:

     

    Ok so the resolution was the boundary thickness (line width) of the

    polygon, combined with the ISOLATE parameter.

     

    ...and the THERMALS property, probably.

     

    It seems strange that there is no granular control of this style -

    the size of the pad and the polygon boundary should be related

    otherwise large pads and small pads on the same polygon behave very

    differently.

     

    If you need different behaviour at different parts of a polygon area,

    simply draw it as more than one (overlapping) polygons with different

    settings. For example, I often combine polygons with and without

    thermals to get the desired copper pour (thermals where necessary for

    soldering, but not where the polygon serves as a heat sink).

     

    Tilmann