Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Part Design: Multiple Chassis Grounds
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 1307 views
  • Users 0 members are here
  • chassis
  • library
  • ground
Related

Part Design: Multiple Chassis Grounds

richardhh
richardhh over 9 years ago

While designing a part recently (a MicroUSB jack, FWIW), I ended up with 6 pads for the chassis ground (4 PTH and 2 SMT pads).

 

Connecting them all to the same signal in the device definition isn't a problem - that's done.  But how do I get Eagle to realize only one needs to be routed (i.e., the pads are already connected to each other within the part)?

 

Right now, Eagle presents 6 airwires - which is fine if the other 5 would clear once the first one gets routed.  I'm hoping not to define just one pad as the routing point, because that'll vary by application (and I'd like them all connected to a plane if it's there).  I suppose I could present 6 swappable chassis pins in the schematic instead of 1.

 

Is there a cleaner solution?

 

Thanks,

Richard

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 30/10/16 01:33, Richard Hornbaker wrote:

    While designing a part recently (a MicroUSB jack, FWIW), I ended up with 6 pads for the chassis ground (4 PTH and 2 SMT pads).

     

    Connecting them all to the same signal in the device definition isn't a problem - that's done.  But how do I get Eagle to realize only one needs to be routed (i.e., the pads are already connected to each other within the part)?

     

    Right now, Eagle presents 6 airwires - which is fine if the other 5 would clear once the first one gets routed.  I'm hoping not to define just one pad as the routing point, because that'll vary by application (and I'd like them all connected to a plane if it's there).  I suppose I could present 6 swappable chassis pins in the schematic instead of 1.

     

    Is there a cleaner solution?

     

    Yes, as of V7.something - earlier versions don't have it, but the

    current version allows you to specify in the library whether a group of

    common pins are to be connected as any or all. Unfortunately the machine

    I'm at has only V5.12 so I can't easily look up the details.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to autodeskguest

    Rob Pearce wrote:

    On 30/10/16 01:33, Richard Hornbaker wrote:

    While designing a part recently (a MicroUSB jack, FWIW), I ended up with 6 pads for the chassis ground (4 PTH and 2 SMT pads).

     

    Connecting them all to the same signal in the device definition isn't a problem - that's done.  But how do I get Eagle to realize only one needs to be routed (i.e., the pads are already connected to each other within the part)?

     

    Right now, Eagle presents 6 airwires - which is fine if the other 5 would clear once the first one gets routed.  I'm hoping not to define just one pad as the routing point, because that'll vary by application (and I'd like them all connected to a plane if it's there).  I suppose I could present 6 swappable chassis pins in the schematic instead of 1.

     

    Is there a cleaner solution?

     

    Yes, as of V7.something - earlier versions don't have it, but the

    current version allows you to specify in the library whether a group of

    common pins are to be connected as any or all. Unfortunately the machine

    I'm at has only V5.12 so I can't easily look up the details.

     

    that feature is available with 6.x already (what x I'm not sure of)

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to autodeskguest

    Rob Pearce wrote:

    On 30/10/16 01:33, Richard Hornbaker wrote:

    While designing a part recently (a MicroUSB jack, FWIW), I ended up with 6 pads for the chassis ground (4 PTH and 2 SMT pads).

     

    Connecting them all to the same signal in the device definition isn't a problem - that's done.  But how do I get Eagle to realize only one needs to be routed (i.e., the pads are already connected to each other within the part)?

     

    Right now, Eagle presents 6 airwires - which is fine if the other 5 would clear once the first one gets routed.  I'm hoping not to define just one pad as the routing point, because that'll vary by application (and I'd like them all connected to a plane if it's there).  I suppose I could present 6 swappable chassis pins in the schematic instead of 1.

     

    Is there a cleaner solution?

     

    Yes, as of V7.something - earlier versions don't have it, but the

    current version allows you to specify in the library whether a group of

    common pins are to be connected as any or all. Unfortunately the machine

    I'm at has only V5.12 so I can't easily look up the details.

     

    that feature is available with 6.x already (what x I'm not sure of)

    --

     

    Lorenz