Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Track thickness list elements
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 474 views
  • Users 0 members are here
Related

Track thickness list elements

jsantosrico
jsantosrico over 9 years ago

When I'm routing new tracks, there is a dropdown with some default values: 10, 12, 16, 24 millis,... When I use a particular thickness, it gets added to the list, but only for the time the program is on, and it resets to the default list upon restarting. I noticed this values are the same in other fields, as it's the case of the text size or via diameter.

 

Is there a way to change it's values to something more useful to me?

 

Also, I noticed that my drill list values in options / set / drills are not the same ones on the dropdown on the via or drill commands. What are those values for? My drill list is in mm, and the values in my dropdown are millis-based.

 

Thanks!

  • Sign in to reply
  • Cancel
  • jsantosrico
    0 jsantosrico over 9 years ago in reply to autodeskguest

    Thanks Jorge,

     

    As usual, you were spot on! Thanks very much!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago

     

    Hello Joel,

     

    I hope you're doing well. You can define your own values by using the

    SET command and adding those entries to your eagle.scr file. The

    eagle.scr file is used to setup defaults in EAGLE since it runs every

    time a new editor is opened.

     

    For example:

     

    SET WIDTH_MENU 0.6mm 1.0mm 1.2mm;

    SET DRILL_MENU 0.6mm 0.8mm 1.0mm 2mm;

     

    See HELP SET for all of the options.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer