Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC Source Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 4411 views
  • Users 0 members are here
Related

AC Source Eagle

ivlaikov
ivlaikov over 9 years ago

     I am new to Eagle. Currently I am using the 7.7 free version on Mac. I want to make a schematic and then export its netlist so that I can use it in MacSpice. However, I can't find a voltage source that can give me a generated wave function with a desired frequency. May you help me?

 

     Thank you in advance!

Ivan Vlaykov

  • Sign in to reply
  • Cancel
  • ivlaikov
    0 ivlaikov over 9 years ago in reply to rachaelp

    This is what I am trying to do now. LTSpice has a mac version as well, but it is alwful that is why I am trying to work it out on MacSpice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ivlaikov
    0 ivlaikov over 9 years ago in reply to autodeskguest

    Thank you for the answer! I didn't know it is possible to create such sort as your own component I will look for help and try to do it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to autodeskguest

    reece wrote on Tue, 27 December 2016 13:41

    Eagle is primarily a PCB layout tool, not a generic schematic capture

    tool for simulation. Since there isn't a physical device like an ideal

    voltage source, you won't find one in the libraries.

     

    This is true but all the big three vendors have well integrated simulation

    add-ons I believe and it makes sense to try to integrate simulation as

    closely with your actual schematics as possible rather than having to draw

    things out several times in different tools. CadSoft sort of integrate with

    LTSpice and did a better job with PCBSim (or whatever it was called) but

    the latter is windows only and the former doesn't yet have a fully working

    export ULP. I think any efforts that bring better integration of EAGLE and

    simulation tools (not just spice but other SI tools, thermal analysis, etc)

    is very worthwhile as it's one of the current weak points in my opinion.

     

    reece wrote on Tue, 27 December 2016 13:41

    Of course there's nothing stopping you from creating such a device in

    your own library and adding it to a schematic.

     

    This is what I would do. I'd create a library especially for simulation and

    add all the source and measure parts into there. These can have various

    attributes associated with them to pass to the simulation tool. I'd also

    add an attribute to any parts in the library that have spice models

    available to specify the model and have a folder in the library to contain

    the models. Finally I would write ULP to export a netlist and some UI add

    in's to interact with MacSpice.

     

    Best Regards,

     

    Rachael

     

    --

    http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 12/25/2016 04:20 AM, Ivan Vlaykov wrote:

    Dear Mr. Garcia,

     

    I am new to Eagle. Currently I am using the 7.7 free version on Mac.

    I want to make a schematic and then export its netlist so that I can

    use it in MacSpice. However, I can't find a voltage source that can

    give me a generated wave function with a desired frequency. May you

    help me?

     

    Thank you in advance! Ivan Vlaykov

     

    Eagle is primarily a PCB layout tool, not a generic schematic capture

    tool for simulation. Since there isn't a physical device like an ideal

    voltage source, you won't find one in the libraries.

     

    Of course there's nothing stopping you from creating such a device in

    your own library and adding it to a schematic.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ivlaikov
    0 ivlaikov over 9 years ago

    Hello Rachael,

     

         Thank you for your answer! I hope the Turkey was nice image.

        

         The thing with MacSpice is that it works only with netlists and doesn't have a greaphical method to put your circuits.

     

    Have great holidays,

    Ivan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago

    Hi Ivan,

     

    I think a lot of people will be eating Turkey today (which will include me shortly!) rather than being on here so you may be out of luck for a quick answer. I use EAGLE on my Mac but unfortunately until your post I didn't know about MacSpice!!! I've now got it installed and will see where I get to with getting it working.

     

    Jorge Garcia from Autodesk is currently working on porting the LTSpice export ULP function to Linux and Mac, currently he's targeting the latest Windows version of LTSpice running under wine for both (as LT haven't updated the Mac version yet). He's probably going to be able to give some advice on how to solve your issue but he's probably out on vacation now I would imagine. I think this might be a good thing to work on an official export ULP for too so maybe we can talk Jorge into adding that to his list while he's got his head around SPICE image

     

    Jorge, you can install MacSpice from Homebrew. Just do: brew install Caskroom/cask/macspice

     

    Anyway, if I find time to have a go with MacSpice myself over the next few days I will post back up if I get anything working.

     

    Best Regards,

     

    Rachael