Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Problem doing thermals. They get swallowed by the Cu pour.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1008 views
  • Users 0 members are here
  • thermals
  • eagle
  • copper
  • thermal
  • pour
  • cu
Related

Problem doing thermals. They get swallowed by the Cu pour.

boojakascha
boojakascha over 9 years ago

Dear Mr. Garcia

 

Today I gave my first ever Gerber files to print. I made those files with EAGLE. However my PCB has no copper pour as I failed to do the thermals right.

I can show my problem in a simple example work flow:

  1. In eagle I choose New/Board
  2. I make a via somewhere
  3. With the “Name tool” I call it GND
  4. I surround it with the “Polygon tool” (thermals enabled, width 0.016 mm)
  5. With the “Name tool” I call the polygon GND
  6. With “Ratsnest” I fill the polygon

This will swallow the via into the copper pour. However I would have expected to have the via somewhat thermally isolated with “thermals”.

Do you know what I am doing wrong? Googling it didn’t solve my issue. I read that it might have something to do with the pin tool. However the pin tool is supposed to be only in the schematic view and not in the board view…

 

With kind regards

Benjamin

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 13/01/17 16:20, Benjamin Spenger wrote:

    Dear Mr. Garcia

     

    Today I gave my first ever Gerber files to print. I made those files with EAGLE. However my PCB has no copper pour as I failed to do the thermals right.

    I can show my problem in a simple example work flow:

    1. In eagle I choose New/Board

    2. I make a via somewhere

    3. With the “Name tool” I call it GND

    4. I surround it with the “Polygon tool” (thermals enabled, width 0.016 mm)

    5. With the “Name tool” I call the polygon GND

    6. With “Ratsnest” I fill the polygon

    This will swallow the via into the copper pour. However I would have expected to have the via somewhat thermally isolated with “thermals”.

    Do you know what I am doing wrong? Googling it didn’t solve my issue. I read that it might have something to do with the pin tool. However the pin tool is supposed to be only in the schematic view and not in the board view…

     

    (Not Jorge here - E14's "ask an expert" simply posts to a forum)

     

    Actually the behaviour you see is correct. Thermals are required so that

    the pad you are attempting to solder a component lead to can get hot

    without all the heat escaping to the ground plane. Vias are not pads,

    they are not expected to have component leads in them, and should never

    need to be soldered. Therefore, they don't get thermals.

     

    Are you attempting to use the via for something other than a via? Should

    you be using a pad instead? Or is your concern over the lack of thermals

    around it misplaced?

     

    Cheers,

    Rob

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 13/01/17 16:20, Benjamin Spenger wrote:

    Dear Mr. Garcia

     

    Today I gave my first ever Gerber files to print. I made those files with EAGLE. However my PCB has no copper pour as I failed to do the thermals right.

    I can show my problem in a simple example work flow:

    1. In eagle I choose New/Board

    2. I make a via somewhere

    3. With the “Name tool” I call it GND

    4. I surround it with the “Polygon tool” (thermals enabled, width 0.016 mm)

    5. With the “Name tool” I call the polygon GND

    6. With “Ratsnest” I fill the polygon

    This will swallow the via into the copper pour. However I would have expected to have the via somewhat thermally isolated with “thermals”.

    Do you know what I am doing wrong? Googling it didn’t solve my issue. I read that it might have something to do with the pin tool. However the pin tool is supposed to be only in the schematic view and not in the board view…

     

    (Not Jorge here - E14's "ask an expert" simply posts to a forum)

     

    Actually the behaviour you see is correct. Thermals are required so that

    the pad you are attempting to solder a component lead to can get hot

    without all the heat escaping to the ground plane. Vias are not pads,

    they are not expected to have component leads in them, and should never

    need to be soldered. Therefore, they don't get thermals.

     

    Are you attempting to use the via for something other than a via? Should

    you be using a pad instead? Or is your concern over the lack of thermals

    around it misplaced?

     

    Cheers,

    Rob

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • boojakascha
    0 boojakascha over 9 years ago in reply to autodeskguest

    Dear Rob

     

    Thanks a lot for your explenations. Yes, you are correct. I should have used pads instead. I will see how the PCBs turned out when they come. Probably I will do them over with pad now that I know :-)