Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Routing board manually, trace will only start at inrouted point.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Subscribers 191 subscribers
  • Views 2196 views
  • Users 0 members are here
Related

Routing board manually, trace will only start at inrouted point.

jelbert
jelbert over 9 years ago

While routing a board, the unrouted (wire unrouted) connections are shown with thin lines.

In the beginning of the board these lines are logical and it helps routing the board. But I can only start a new trace at the point where these thin lines start.

image

At this example I want to start routing at the end of the GND trace. But the router will not allow me to do that. The workaround is to delete the trace to the point of the unroute and then continue from there. In this case that is not much extra work. But sometimes I have to delete quite a lot until I can continue.

There must be a setting somewhere to disable this 'feature' and let me route from any point I want. But how?

I use Eagle 7.7 Premium.

  • Sign in to reply
  • Cancel
Parents
  • c4m4ch0
    0 c4m4ch0 over 9 years ago

    Hi, I usually do the same and delete a part of the net and start routing again there but when it cames to gnd, normally I use the polygon tool to do a gnd plane to save me time instead of trace all the grounds. Also its quicker to etching the pcb and keep your circuit more immune to interference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • c4m4ch0
    0 c4m4ch0 over 9 years ago

    Hi, I usually do the same and delete a part of the net and start routing again there but when it cames to gnd, normally I use the polygon tool to do a gnd plane to save me time instead of trace all the grounds. Also its quicker to etching the pcb and keep your circuit more immune to interference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jelbert
    0 jelbert over 9 years ago in reply to c4m4ch0

    But it can not be true that this is the only way to route a trace! I used other routing software ,Mentor Graphics Pads, and never had this kind of problem. There you had the same lines. But when clicking on a net the line would jump to that place on the net and routing would start from that point.

    Eagle has the great advantage of the ULP language and the use of eagle in the Open Source community.