Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Add holes for through hole components
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 7 answers
  • Subscribers 190 subscribers
  • Views 8135 views
  • Users 0 members are here
Related

Add holes for through hole components

ardenne
ardenne over 9 years ago

Hi, I am new in the Eagle world and I am making a 2 layers custom board with Eagle. 

I am trying to do a simple custom size board full of holes for through hole components ( a simple prototyping board) and I am not sure about which is the best way to make the holes.

I have found many resources with totally different answers. For example on this video: https://www.youtube.com/watch?v=s4-Ugi4y9lk (min: 24.00) this guy use the simple command VIA for doing this, but a VIA should be just a connection between layers.  On this discussion How to add connection points for soldered wires , another guy suggest instead the library wirepad.lbr.

This is a working project. not for fun, so I need to be quite sure that I am making the righ hole. Could you someone help me? It will be really appreciate.

  • Sign in to reply
  • Cancel
  • geralds
    0 geralds over 9 years ago

    Hi Angela,

     

    Holes, pad:
    Well, in the schematic or pcb you have 3 types of holes (round eg drilling, square eg punching, complex eg milling) that are separated into plated or non-plated holes.

    A via yes is, of course, also a plated hole, but its using is a bit different.

     

    In the schematic - ADD from the library, you can choose from:

    Holes.lbr (mounting holes, non plated or plated, round or square, or even complex special hole)
    Solpad.lbr (solderable pads, but this lbr is very inflexible)
    Wirepad.lbr (solderable pads, through holes with type of hole diameters and rings, also SMD pads)
    Or you can create your own lbr file with your pads or holes.

     

    If you use ADD in pcb i strongly suggest that you imports just holes, but not pads if they are will connected to an electrical contact.

    If you likes importing pads then make this into the schematic, also better importing the holes into the schematic.

    (-> consistence between schematic and pcb)

     

    The point:
    PAD is basically a plated hole or a SMD pad
    HOLE is basically a non-plated hole, is only for assembly or for the distances, e.g. for high-voltage security distance.

    For your project I suggest you to make your own lbr file. You can also copy the default pads into your lbr file.
    Please also read the manual and the tutorial. There you will find nice examples.

     

    Via:
    A plated hole used in the circuit board to connect through and between the layers.
    They can also be very flexible.

    If you want to connect some of the vias to a wire, you must use the command: NAME

    Then the menu will ask you: "this segment or complete wire" -> use complete wire!

     

    Power plane:
    Power planes are usually created by drawing a polygon, and then this polygon will connected to an electrical wire.
    (E.g. GND or VCC or VDD, .... or N $ xxx

    -> and if pads or vias are connected to this wire, then the polygon includes it in its calculation.

     

    Best Regards,

    Gerald

    ---

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to autodeskguest

    Lorenz wrote on Thu, 02 March 2017 06:59

    But for the pads without connections, use plain vias.

    They are inserted/placed in the board only.

    You can still connect this vias with the connect command (in the board

    editor - to form a GND rail for instance)

     

     

    Are you sure? I thought the connect command was used in the library editor

    to connect pads to pins in a part? I think in this case you'd want to use

    the name command to name any vias you wanted to be connected together to

    the same net or simply add them with a name already set.

     

    e.g. name 'GND' or via 'GND'

     

    I'd suggest that if you really wanted any of the holes connected you'd want

    to have a schematic and connect them there though rather than doing it all

    in the board so if this was the case the wirepad.lbr option would probably

    be the correct option.

     

    Best Regards,

     

    Rachael

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago

    Angela Ameruoso wrote:

     

    Hi, I am new in the Eagle world and I am making a 2 layers custom board with Eagle. 

    I am trying to do a simple custom size board full of holes for through

    hole components ( a simple prototyping board) and I am not sure about

    which is the best way to make the holes.

     

    depends 8-)

     

    for pads that need a connection in the schematic you can use

    wirepad.lib parts.

    They need to be i nserted in the schematic.

     

    But for the pads without connections, use plain vias.

    They are inserted/placed in the board only.

    You can still connect this vias with the connect command (in the board

    editor - to form a GND rail for instance)

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<