Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Hierarchical Component Numbers on PCB - how to renumber/get rid of module prefix?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 1568 views
  • Users 0 members are here
Related

Hierarchical Component Numbers on PCB - how to renumber/get rid of module prefix?

pieters
pieters over 9 years ago

Hi

Please advise how one could switch of the <MODULE>:<NUMBER> type numbering of components on PCB's? to only show the <NUMBER> - as well as how to renumber across hierarchical designs?

 

Regards,

  • Sign in to reply
  • Cancel
  • Richard_H
    0 Richard_H over 9 years ago in reply to rachaelp

    On 2017-05-05 09:52:45 +0000, rachaelp said:

     

    Richard Hammerl wrote:

     

    Hi Rachael,

     

    no this is not new. It came with V7 and the hierarchical design. Don't

    know why you missed it.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    Autodesk -- EAGLE Support

    Hi Richard

     

    I'd read through the help on the hierarchical design functionality

    previously so I thought I would have noticed this! Was is maybe not

    fully documented initially and only updated at a later time? I'm

    clutching at straws here as to why I missed something so obvious!

     

    However, even though it does allow the NAME:REFDES format to be reduced

    to just REFDES, because of the way it works on anything but the

    simplest of designs with one or two modules it'll be next to unusable

    without creating loads of conflicts, especially when modifying designs

    at a later date and adding new instance of existing modules, I think

    it'll just end up a mess. Would it be possible to give the option so

    that parts within modules get renumbered as if they were part of a flat

    design please? This would make the hierarchical design functionality

    really useful for larger designs, where it would actually give the most

    benefit.

     

    I'll also pop something up as a suggestion in the new Autodesk EAGLE

    forums at some point, along with some other suggestions I have for

    improving hierarchical design.

     

    Best Regards,

     

    Rachael

     

    Hi Rachel,

     

    we know that there have to be improvements with hierarchical design.

    There are already plans made how it has to look like. At the moment I

    do not know exactly what the changes will be, but I am sure that our

    support team noticed your post and will draw conclusions of it.

     

    Have a great day.

    Richard

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    Autodesk -- EAGLE Support

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to Richard_H

    Richard Hammerl wrote:

     

    Hi Rachael,

     

    no this is not new. It came with V7 and the hierarchical design. Don't

    know why you missed it.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    Autodesk -- EAGLE Support

    Hi Richard

     

    I'd read through the help on the hierarchical design functionality previously so I thought I would have noticed this! Was is maybe not fully documented initially and only updated at a later time? I'm clutching at straws here as to why I missed something so obvious!

     

    However, even though it does allow the NAME:REFDES format to be reduced to just REFDES, because of the way it works on anything but the simplest of designs with one or two modules it'll be next to unusable without creating loads of conflicts, especially when modifying designs at a later date and adding new instances of existing modules, I think it'll just end up a mess. Would it be possible to give the option so that parts within modules get renumbered as if they were part of a flat design please? This would make the hierarchical design functionality really useful for larger designs, where it would actually give the most benefit.

     

    I'll also pop something up as a suggestion in the new Autodesk EAGLE forums at some point, along with some other suggestions I have for improving hierarchical design.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 9 years ago in reply to rachaelp

    On 2017-05-04 13:36:00 +0000, rachaelp said:

     

    Richard Hammerl wrote:

     

    you can change the naming of components (not of the signals) in

    hierarchical designs,

    if you define an "Offset" in the Properties of the module instance.

    See HELP MODULE.

     

     

    Hi Richard,

     

    Is this new functionality? If not how did I miss this previously?! It's

    not perfect but it certainly makes things possible for some smaller

    designs.

     

    The problem will come when trying to do large designs with multiple

    different modules. I think it'll rapidly become impossible to get this

    to work without causing part number conflicts. For this reason, having

    the option to just number parts as if it were a flat design but

    maintain the ability to manipulate as a hierarchical block would make

    this much more useful.

     

    Best Regards,

     

    Rachael

     

    Hi Rachael,

     

    no this is not new. It came with V7 and the hierarchical design. Don't

    know why you missed it.  image

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    Autodesk -- EAGLE Support

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to Richard_H

    Richard Hammerl wrote:

     

    you can change the naming of components (not of the signals) in

    hierarchical designs,

    if you define an "Offset" in the Properties of the module instance.

    See HELP MODULE.

     

     

    Hi Richard,

     

    Is this new functionality? If not how did I miss this previously?! It's not perfect but it certainly makes things possible for some smaller designs.

     

    The problem will come when trying to do large designs with multiple different modules. I think it'll rapidly become impossible to get this to work without causing part number conflicts. For this reason, having the option to just number parts as if it were a flat design but maintain the ability to manipulate as a hierarchical block would make this much more useful.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 9 years ago

    Hi,

     

    you can change the naming of components (not of the signals) in

    hierarchical designs,

    if you define an "Offset" in the Properties of the module instance.

    See HELP MODULE.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    Autodesk -- EAGLE Support

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pieters
    0 pieters over 9 years ago in reply to rachaelp

    Thanks - appreciate the answer

     

    I've changed the module/hierarchical structure back to a flat structure.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago

    Pieter Swanevelder wrote:

     

    Please advise how one could switch of the <MODULE>:<NUMBER> type numbering of components on PCB's? to only show the <NUMBER> - as well as how to renumber across hierarchical designs?

    Unfortunately this is not currently possible, it's one of the major drawbacks with the way module functionality is implemented. The best thing you can do at the moment is name your modules with really concise names so that your reference designator length is minimized but even then, on dense boards with small components, even with the tiniest of writing, it can be impossible to place everything so you have a tidy and readable silkscreen. For me this issue (amongst several others if I am being honest) has severely limited the usefulness of this feature to me in my designs.

     

    Best Regards,

     

    Rachael