Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) SMD on single sided board with Through Hole components?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 2574 views
  • Users 0 members are here
Related

SMD on single sided board with Through Hole components?

augustoagc
augustoagc over 9 years ago

Hello. I'm new here as well as a new Eagle user.

Going straight to the point, I'm just a hobbyist. I transfer muy pcbs using transfer paper.

 

The thing is that I now need to use some SMD components on a pcb I'm making that also has through hole components. What I usually do is print the PCB unmirrored and transfer it to the PCB. That way, I can mount the components from the back. That is, solder from the bottom of the PCB. However you want to look at it.

Now that I have SMDs, I need the SMD pad, and only that, to be mirrored at the time of printing so that, when I transfer, it only this is left unmirrored.

But when I mirror a component, Eagle sends it to the bottom layer. And there is nothing I can do (that I know of) to bring it back to the top layer in this state. The only way is to unmirror it.

So basically, Eagle is forcing me to do a two layer PCB when a single layer is more than enough.

 

I hope I was clear enough... if not please ask,

Thank you!

  • Sign in to reply
  • Cancel
  • augustoagc
    0 augustoagc over 9 years ago in reply to autodeskguest

    ...Here's an attachment that I made to help explain myself. I know I'm

    perhaps not being clear...

    I want to have all the components on one side and route them on that side

    (perhaps this is not possible)...

     

    Yes I made a mistake there. What I need is really what I drew in the attachment.

     

    And here's the answer:

     

    If you want all through hole components mounted on the top and soldered to

    the traces on the bottom and any SMD mounted on the bottom, as they must be

    when all the traces are on the bottom then. Route on the bottom layer and

    mirror SMD components to the bottom. Print without mirroring for toner

    transfer.

     

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to augustoagc

    ...Here's an attachment that I made to help explain myself. I know I'm

    perhaps not being clear...

    I want to have all the components on one side and route them on that side

    (perhaps this is not possible)...

     

    I think you have made an error in your diagram saying this is what you want

    and yet in your writing you say "I want to have all the components on one

    side and route them on that side". The diagram does not show that

    combination.

     

    So for toner transfer, if you want all the components, both through hole

    and smd mounted on the top then you design the board with the through hole,

    SMD and routing on the top layer with no components mirrored and then print

    mirrored. You will need to ensure all through hole components can be

    soldered from the top.

     

    If you want all through hole components mounted on the top and soldered to

    the traces on the bottom and any SMD mounted on the bottom, as they must be

    when all the traces are on the bottom then. Route on the bottom layer and

    mirror SMD components to the bottom. Print without mirroring for toner

    transfer.

     

    HTH

    Warren

     

     

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • augustoagc
    0 augustoagc over 9 years ago in reply to autodeskguest

    Thank you Warren. Sorry for the (big) delay. As I said this is my hobby and so I don't have as much time as I'd like for it ...

    I understand what you propose. I should mirror the SMDs (they would then be on the bottom layer) and route. Then print the top layer and bottom layer stacked and transfer them to a single-layer PCB.

    However, I'd have to make sure no routes intersect between layers...

    Here's an attachment that I made to help explain myself. I know I'm perhaps not being clear...

    I want to have all the components on one side and route them on that side (perhaps this is not possible).

    Thank you for your help!

    Attachments:
    imageExpl.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to autodeskguest

    On 5/06/2017 3:45 p.m., warrenbrayshaw wrote:

     

     

    ..........Then you print the lower layer mirrored so its correct for toner transfer.

     

    HTH

    Warren

     

     

    Woops -  mistake!

    No need to mirror the print for the toner transfer

     

    You would mirror it if producing a component placement diagram for the

    bottom view.

     

    HTH

    Warren

     

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

    ... or http://www.eaglecentral.ca browser access to CadSoft EAGLE

    support forums.

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 5/06/2017 3:11 p.m., Augusto Garcia Cinselli wrote:

    Hello. I'm new here as well as a new Eagle user.

    Going straight to the point, I'm just a hobbyist. I transfer muy pcbs using transfer paper.

     

    The thing is that I now need to use some SMD components on a pcb I'm making that also has through hole components. What I usually do is print the PCB unmirrored and transfer it to the PCB. That way, I can mount the components from the back. That is, solder from the bottom of the PCB. However you want to look at it.

    Now that I have SMDs, I need the SMD pad, and only that, to be mirrored at the time of printing so that, when I transfer, it only this is left unmirrored.

    But when I mirror a component, Eagle sends it to the bottom layer. And there is nothing I can do (that I know of) to bring it back to the top layer in this state. The only way is to unmirror it.

    So basically, Eagle is forcing me to do a two layer PCB when a single layer is more than enough.

     

    I hope I was clear enough... if not please ask,

    Thank you!

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/223493

     

     

     

    Hi

    Your description is less than clear so maybe the following will help.

    Eagle is always a view from the top through the board.

     

    Conventionally, if you were to design a one layer board with through

    hole components you would place the components on the top side and

    solder on the bottom layer. All your tracks (routing) are on the bottom

    layer and hence any SMD will need to be there as well.

     

    So for an SMD on the bottom layer, you need to mirror them. This has the

    effect of making then present correctly (pin wise) as you view the board

    from the top.

     

    Then you print the lower layer mirrored so its correct for toner transfer.

     

    HTH

    Warren

     

     

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

    ... or http://www.eaglecentral.ca browser access to CadSoft EAGLE

    support forums.

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer