Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Can't place some points in the command line. Invalid point
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 190 subscribers
  • Views 2176 views
  • Users 0 members are here
  • command
  • line
  • invalid
  • point
  • error
Related

Can't place some points in the command line. Invalid point

s0s
s0s over 9 years ago

Edit: Adding this line: I can't place points in the command line when I try to place pads in the package editor.

 

I have Eagle 6.5.0 Light for 64-bit Mint Linux. I want to place 32 pads in the package editor. I've calculated all the points, and it would be much faster if I could place them in the command window, because they would be accurate. This link shows it can be done: Cadsoft Eagle how to make parts tutorial - DP

 

I notice the bug is when both coordinates are negative. However, the author of the article I linked to suggests making some negative, so that the package will be centered. I can manually place the points, but it's a real pain to get it to be accurate. Does anyone know how to solve this? I have done searches, but I saw no relevant results.

 

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 21/06/17 23:16, s0s wrote:

    I want to place 32 pads in the package editor. I've calculated all the points, and it would be much faster if I could place them in the command window, because they would be accurate. This link shows it can be done: Cadsoft Eagle how to make parts tutorial - DP (http://dangerousprototypes.com/docs/Cadsoft_Eagle_how_to_make_parts_tutorial)

     

    I notice it's when both coordinates are negative. However, the author of the article I linked to suggests making some negative, so that the package will be centered. I can manually place the points, but it's a real pain to get it to be accurate. Does anyone know how to solve this? I have done searches, but I saw no relevant results.

     

    Thanks in advance.

     

    Sorry, but in your enthusiasm to say when your problem happens, you appear to

    have omitted to say what your actual problem is!

     

    The link you referenced gives the following example:

     

    (-1 -2.4)(-.5 -2.4)(0 -2.4)(.5 -2.4)(1 -2.4)(1 2.4)(.5 2.4)(0 2.4)(-.5 2.4)(-1 2.4);

     

    As long as you follow that format (I prefer to add spaces between coordinate

    pairs but Eagle probably isn't fussed) then it should work. What are you

    actually typing in?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • s0s
    0 s0s over 9 years ago in reply to autodeskguest

    The problem is described in the title of this topic. I can't place some points (when I'm trying to add pads in the package editor). I've added a line to the top of the post above to clarify. When both the x and y coordinate are negative, it refuses to place the pad at that point from the command line.

     

    I attempted exactly what you did, and it did not work. I even tried doing a single point. But again, if both coordinates are negative, it won't do it. I had to waste time manually putting them where I want them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to s0s

    Hello,

     

    I do this in my scripts regularly and it does work fine for me, but I am using a much newer version of EAGLE.

     

    As you are using a freeware version (linux repos don't have anything newer than v6) I would recommend that you download either the latest v8 version (requires an Autodesk account) from http://cadsoft.io or alternatively if you don't have/want an Autodesk account to run EAGLE then download the most recent v7 version from http://eagle.autodesk.com/eagle/software-versions

     

    At the very least if you don't want to move forward from v6 you should get the very latest v6.6 version which is also available from the Autodesk link above.

     

    So I have just used your failing points list from above and using the package editor from v8.2.2 I executed:

     

    SMD (-1 -2.4)(-.5 -2.4)(0 -2.4)(.5 -2.4)(1 -2.4)(1 2.4)(.5 2.4)(0 2.4)(-.5 2.4)(-1 2.4);

     

    It correctly placed two rows of pads as expected.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • s0s
    0 s0s over 9 years ago in reply to rachaelp

    It works in a different file. I don't know why it wouldn't work before, but I'm done with that now, so I'm not going to worry about it. I'm designing a board now, and it worked in this file, so who knows. I want to thank everyone who sincerely tried to help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • s0s
    0 s0s over 9 years ago in reply to rachaelp

    It works in a different file. I don't know why it wouldn't work before, but I'm done with that now, so I'm not going to worry about it. I'm designing a board now, and it worked in this file, so who knows. I want to thank everyone who sincerely tried to help.