Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Problems creating an PCB track NFC antenna
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 3654 views
  • Users 0 members are here
  • eagle
  • pcb antenna
Related

Problems creating an PCB track NFC antenna

Fred27
Fred27 over 8 years ago

I'm trying to create a PCB track NFC antenna as an Eagle part. As part of this I need a via so I can bring out the connection from the centre of the coil. Is it possible in a library part?

 

Also, the antenna involves a trace which appears to "short" two nets, so I get an overlap DRC error. Is it possible to avoid this?

 

I took a look at Sparkfun's RFID evaluation shield to see if that gave me any clues. They apparently went for the antenna as part of the design rather than a library part (avoiding the via issue) but still appear to have similar overlap errors.

https://www.sparkfun.com/products/10406

  • Sign in to reply
  • Cancel
Parents
  • berniwa
    0 berniwa over 8 years ago

    Hey David,

     

    it is much simpler if you do the antenna in the board and not in the library, as you can do a design without the mentioned DRC errors.

     

    It basically just:

    1. Short the pins out in schematics.

    image

     

    2. Draw the  antenna wires as suggested in the design note of the NFC IC.

    image

     

    A few tips when working with NFC:
    In order for the antenna to work properly you'll need to individually match to your antenna, and in most cases you won't get away with the matching from another design.
    So make sure, to have a least two footprints (0805, 0603 or 0402) for each matching component, this will allow you to solder capacitors in parallel what allows you to to trial and error test matching easier.

     

    Greets

    Berni

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Fred27
    0 Fred27 over 8 years ago in reply to berniwa

    Thanks for the tips. I was trying to add the antenna as an Eagle part so that I could reuse it in other designs. However, it looks like this is more trouble than it's worth. I'll just create it as part of the board and copy it if needed.

     

    I'm aware of the need for matching. I have a guide about how to do matching without a VNA - I hope that will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Fred27
    0 Fred27 over 8 years ago in reply to berniwa

    Thanks for the tips. I was trying to add the antenna as an Eagle part so that I could reuse it in other designs. However, it looks like this is more trouble than it's worth. I'll just create it as part of the board and copy it if needed.

     

    I'm aware of the need for matching. I have a guide about how to do matching without a VNA - I hope that will work.