Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Problems creating an PCB track NFC antenna
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 3658 views
  • Users 0 members are here
  • eagle
  • pcb antenna
Related

Problems creating an PCB track NFC antenna

Fred27
Fred27 over 8 years ago

I'm trying to create a PCB track NFC antenna as an Eagle part. As part of this I need a via so I can bring out the connection from the centre of the coil. Is it possible in a library part?

 

Also, the antenna involves a trace which appears to "short" two nets, so I get an overlap DRC error. Is it possible to avoid this?

 

I took a look at Sparkfun's RFID evaluation shield to see if that gave me any clues. They apparently went for the antenna as part of the design rather than a library part (avoiding the via issue) but still appear to have similar overlap errors.

https://www.sparkfun.com/products/10406

  • Sign in to reply
  • Cancel
Parents
  • geralds
    0 geralds over 8 years ago

    Hi David,

     

    For more information how to design an PCB printed antenna you can find it here, for example:

    https://www.autodesk.com/products/eagle/blog/rfid-works-antenna-design/

     

    Here you'll find a reference design:

    http://www.st.com/content/ccc/resource/technical/document/application_note/d9/29/ad/cc/04/7c/4c/1e/CD00221490.pdf/files/…

     

    Here there are some chip manufacturer they makes RFID chips and also have their reference designs.

    www.ti.com

    www.maximintegrated.com

    www.microchip.com

    www.atmel.com (microchip)

    www.silabs.com

    www.cypress.com

     

    In the Eagle you can make PCB printed coils with the print-inductor.ulp

    Just click in the PCB on the menu item "tools" and "calculate printed-coils", then a menu window pops up with that you can create your printed inductor.

    imageimage

     

    --

    Or there is also the ulp - spiral-coil.ulp what you can use for.

    Click in the PCB on the button ULP: select the file spiral-coil.ulp

    image

    (this is a bit older and smaller ulp file but it works fine)

     

    As suggested, yes, you also needs parts for the impedance correction.

     

    Best Regards,

    Gerald

    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • berniwa
    0 berniwa over 8 years ago in reply to geralds

    Hey,

     

    I wouldn't use the calculator ulps though, as it is much easier to draw two windings by hand (and more are in most cases not neceassary) than to fiddle with the calculator.

     

    Greets

    Berni

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • berniwa
    0 berniwa over 8 years ago in reply to geralds

    Hey,

     

    I wouldn't use the calculator ulps though, as it is much easier to draw two windings by hand (and more are in most cases not neceassary) than to fiddle with the calculator.

     

    Greets

    Berni

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • geralds
    0 geralds over 8 years ago in reply to berniwa

    Hi,

     

    Yes, i would it draw too. But, after that if doesn't work correct, you can build it once more.image

     

    Greets

    Gerald

    ---