EAGLE User Support (English) Auto-Routing Double Sided Board with non Plated Through Holes
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
  • State Verified Answer
  • Replies 12 replies
  • Answers 3 answers
  • Subscribers 181 subscribers
  • Views 2055 views
  • Users 0 members are here
  • autorouter
  • hand-crafted
  • eagle ulp
  • double side
  • pth
  • eagle autorouter
Related

Auto-Routing Double Sided Board with non Plated Through Holes

antzy
antzy over 8 years ago

As a hobbyist, I find it much faster for prototyping make my own boards and recently got a CNC router to speed up prototyping. I usually route the boards myself but sometimes don't have enough time to do it by hand. The problem is that while the auto-router works fine for hand-made single sided boards, for double-sided boards, there is no way to turn off PTH for the pads. It will always assume the top and bottom of all pads to be connected by default and route accordingly. As everyone knows, making PTH at home is not feasible(time and money).

Is there any setting to tell the auto-router not to assume pads' top and bottom to be connected?

One way I see is by using a ULP that places pads' duplicate shapes on bRestrict for parts on bottom side and on tRestrict for parts on the top side. Is there any such ULP available?

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +2 suggested
    Antzy, A super simple way to deal with the through holes is to just feed a small wire through the 'via' holes and solder the wire top and bottom. Instant plated through hole! Gene
  • antzy
    antzy over 8 years ago in reply to genebren +1 suggested
    That works for vias but not for pads. For pads, the only way to connect top and bottom is by soldering on both sides and that isn't possible for most components (ICs, electrolytic capacitors, headers,…
  • genebren
    genebren over 8 years ago in reply to antzy +1
    Antzy, That is a good point. I do not have the auto-routing feature on my software (license) so I can not test any of the settings. Even when I did have the correct license, I found that the auto-router…
  • genebren
    0 genebren over 8 years ago in reply to antzy

    Way to go!  That was some nice work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • antzy
    0 antzy over 8 years ago in reply to genebren

    Thank you Gene! Thanks to you, Warren and Paul, I kept at it, else would have given up long ago.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<