EAGLE User Support (English) Move Part / Device to Other Layer (Bottom)
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
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 5117 views
  • Users 0 members are here
Related

Move Part / Device to Other Layer (Bottom)

phased
phased over 8 years ago

Hello,

 

I have been working on a PCB design which is intended to use an edge card connector. I first created a package / symbol / device which represented this connector as having copper (fingers) on both the top and bottom layers. However, when attempting to export the routing files to a manufacturing house, I got a failure message with errors such as: Your project doesn't contain a bottom copper file and Your project doesn't contain a bottom solder mask.

So this made me realize that, even though I created the package to have copper on both Top and Bottom layers, the board layout kept both sets of copper on the Top layer.

 

After this, I attempted to create a device which had only one set of fingers so I could put device on the Top layer and another on the Bottom layer. However, apparently Eagle will not allow me to put a device on the Bottom layer.

 

Can anyone tell me if there is something special I need to do to accomplish this or if I am going about the process of adding edge connector fingers to a board incorrectly and how I may do it differently?

 

Thank you very much in advance!

 

Troy.

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 8 years ago +1 suggested
    Am 22.03.2018 um 17:30 schrieb Troy Whipple: Hello, I have been working on a PCB design which is intended to use an edge card connector. I first created a package / symbol / device which represented this…
  • autodeskguest
    0 autodeskguest over 7 years ago

    Troy Whipple wrote:

    However, when attempting to export the routing files to a

    manufacturing house, I got a failure message with errors such as: Your

    project doesn't contain a bottom copper file and Your project doesn't

    contain a bottom solder mask.

     

    You have set up your board to have a top and a bottom layer in DRC?

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phased
    0 phased over 7 years ago in reply to autodeskguest

    Hello Paul,

     

    Thank you very much for your reply. I was able to mirror the part I was having trouble with after moving it to an area of the board that allowed for it to not go 'out of bounds'.

     

    I appreciate your help!

     

    Troy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<