Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) What is the right width of trace should I choose for 220VAC
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 10 answers
  • Subscribers 190 subscribers
  • Views 5810 views
  • Users 0 members are here
  • high voltage
  • trace-width
  • pcb trace
  • eagle 9.0.0
Related

What is the right width of trace should I choose for 220VAC

anthonylauly
anthonylauly over 8 years ago

image

Hi, I want to design a pcb that convert AC (220VAC) to DC (10 V), so I would use a wider trace for the Neutral and Line. First I would like to know what is the measurement unit use in the radius and width toolbox, second what is the difference of the radius and width of the trace, because when I increase the radius, nothing is happen. Third, what is the right number of radius and width for 220 VAC, thank you.

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 8 years ago

    Hi Anthony,

     

    I'm going to start by a very strong word of caution. Please be extremely careful when working with mains voltages. If you don't know you can do something safely or are unsure in any way then don't proceed.

     

    So, that said, you say 10V output but you don't state the current requirements. What are they? What is the power supply type? Is it linear? Is it switching? All these things will affect the current required on the mains input. It's the current requirement which drives the required trace width. On the other hand, the voltage drives the required separation which must be maintained between the live and neutral traces, and also to any other traces, not just the continuous mains voltage but any safety standards which require a particular level of isolation. See the following link for some further explanation: http://www.ni.com/white-paper/2827/en/

     

    For the clearances specified in IPC-2221 take a look at the following link: http://www.smpspowersupply.com/ipc2221pcbclearance.html

    To calculate the trace widths required take a look at the following link: http://circuitcalculator.com/wordpress/2006/01/31/pcb-trace-width-calculator/

     

    You don't need to worry about the radius setting in the route tool in EAGLE for now, that's for mitred corners. You can use that to smooth out 45 and 90 degree bends if you wish though.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anthonylauly
    0 anthonylauly over 8 years ago in reply to rachaelp

    If I have this kind of circuit  :

    image

    That what is the trace width should I use from the N and L that is connected to the diode bridge ? Because I cannot measure the current flow. The output for the diode bridge is 2 Ampere. Then what is the trace width should I choose ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to anthonylauly

    Hi Anthony,

    You might need to check out the design of your circuit. As drawn the maximum current that it will draw is 2 mA. R1 100K and R3 10K are in series with the regulator. The data sheet on the LM317 indicates that it needs at least 3.5 mA load to maintain regulation and the circuit as drawn can not deliver more than 2 mA and this would be in a default state where the input of the LM317 is shorted to ground. To accomplish what you want to do you will best use a transformer with a 220 volt primary and a 12 volt secondary, then the bridge rectifier and then directly into the input of the LM317 without R1, R2, or R3. C1 and C2 can be combined and should be a lot bigger like 4700 uF if you want to keep ripple down at 2 amps draw. Back to your original question, if 2 amps at 10 volts is being delivered to the load then the 220 volts will be supplying roughly a tenth of an Amp and the traces to the transformer primary will not need to be over sized.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to autodeskguest

    Hi Warren,

    Thanks for your good input. FYI these EAGLE questions also show up on the element 14 forum where we routinely answer nuts and bolts questions. Most of the times they are about CAD problems but sometimes, like this one, they demand a response.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago in reply to autodeskguest

    Hi Warren,

    Thanks for your good input. FYI these EAGLE questions also show up on the element 14 forum where we routinely answer nuts and bolts questions. Most of the times they are about CAD problems but sometimes, like this one, they demand a response.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer