Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) how to find invisible pins?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 778 views
  • Users 0 members are here
  • invisible pins
  • delete pins
  • delete pads
Related

how to find invisible pins?

nikodemus
nikodemus over 8 years ago

Hi,

I want to use an Arduino Nano on my board by plugging it into sockets on my board, i.e. the USB connector and the ICSP pins have no direct connection to my board.

There is a device for the Nano in the "E14_Arduino_revC.lbr" from Element14. This device contains pins/pads for the USB connector and the ICSP. Using this device my board will have pads for USB and pads for ICSP. To use the area below the Nano for wiring on my board these pads shall be removed. And here comes the problem.

 

I could remove the pads for USB after disconneting them from their pins, deleting the pins in the symbol editor and then deleting the pads in the package editor.

But the symbol does not contain pins for ICSP, i.e. they are not visible. After clicking on the "connect" button the pins for ICSP are listed and can be disconnected. But I cannot delete these pins in the symbol editor because they are not visible.

 

How can I delete these pins for ICSP?

  • Sign in to reply
  • Cancel
Parents
  • WarrenBrayshaw
    0 WarrenBrayshaw over 8 years ago

    Hi

    I suspect you do not have the layer 'pins' visible..

    Use the mouse to activate the Pins layer or type the following into the command line.and then hit <ENTER>

     

    DISPLAY PINS

     

    HTH

    Warren

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • WarrenBrayshaw
    0 WarrenBrayshaw over 8 years ago

    Hi

    I suspect you do not have the layer 'pins' visible..

    Use the mouse to activate the Pins layer or type the following into the command line.and then hit <ENTER>

     

    DISPLAY PINS

     

    HTH

    Warren

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • nikodemus
    0 nikodemus over 8 years ago in reply to WarrenBrayshaw

    Hi,

    yes, after disconnecting the pins and displaying the pins with your command, they were visible and could be deleted as well as the pads.

    Thank you