Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Flounder meets the CONNECT command (and loses)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 886 views
  • Users 0 members are here
  • connect command
  • eagle 9
  • newbie
Related

Flounder meets the CONNECT command (and loses)

supuflounder
supuflounder over 8 years ago

I'm feeling more like Bambi in "Bambi meets Godzilla".

 

I have a symbol.  I gave the pins name like NOA, COMA, NCA (yes, it's a relay!  A genuine metal-on-metal contact set.  There are sound reasons for this, mostly dealing with forward voltage drop across MOSFETs messing up the circuit and also limiting the total current draw due to their resistance).  I spent most of the  night switching between various tutorials and Eagle.  I have pads, and the pads have names like P$2, P$3, etc.  Then I get to the Device level, and want connect something like P$4 with NOA, P$5 to COMA, and P$6 to NCA (no, I don't remember the pin mappings, and I want to go to bed...).  What I expected is what is shown in all the tutorials. What I get is a dialog with an empty pin list, as shown in the attached screenshot.  Just to show the the device has pin names (which I renamed from P$1, etc.), I show the symbol view.  But I put the pins down, then renamed them.

 

I really am a newcomer to Eagle; I've been using it less than a week, and this is my first attempt to create a part.  I feel that i understand enough about .brd and .sch to make progress, albeit more slowly than an expert, but there aren't any prebuilt libraries I could find for this part, so decided that it was time to stretch my understanding and build my own part.

 

I am using 9.1.1, which was current when I started last week; 9.1.2 is now out, but I have not yet upgraded.

 

The tutorials I've found are clear, but they all end up with a set of pins to be connected to a set of pads.  I have no set of pins, and do not understand why. I would appreciate if someone could point out what I've done wrong and/or tell me how to fix it.

 

Also, the only file I found was a .lbr file; I presume it contains both the .sch and .brd components magically within itself.  And when I add it, it includes the file with the #1 in its name.  I am too tired to worry about that right now. [If it does not appear, it is because I got an error message about "The content type of this file" not being a permitted attachment.  Typical sloppy work; a real message would have given the file name, since I had four attachments.  Or, it would have highlighted the forbidden attachment.].

 

      joe

(aka "The Supuflourous Flounder)

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 8 years ago

    Hello,

     

    From the first screenshot it appears you have no added the symbol to the device hence it’s pins are not showing in the connect dialog.

     

    I wrote a library creation tutorial a while back. You should be able to find it if you do a searchfor eagle tutorial in the search here.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 8 years ago

    Hello,

     

    From the first screenshot it appears you have no added the symbol to the device hence it’s pins are not showing in the connect dialog.

     

    I wrote a library creation tutorial a while back. You should be able to find it if you do a searchfor eagle tutorial in the search here.

     

    Best Regards,

     

    Rachael