Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) programming ATTiny85 with arduino pro mini
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 1460 views
  • Users 0 members are here
Related

programming ATTiny85 with arduino pro mini

gub11
gub11 over 10 years ago

I am using the arduino IDE and the arduino pro mini as an isp for my ATTiny85.  I am trying to test out the functionality of the tiny with a simple blink circuit, but first i obviously need to put the code on it.  I have all the wires going to and from the correct pins on my attiny and pro mini, but whenever i  upload to the attiny, with the pro min as an isp, i get the error unidentified device signature 0x0000000.

What should i do?

  • Sign in to reply
  • Cancel

Top Replies

  • screamingtiger
    screamingtiger over 10 years ago +1
    are you using a FDTI serial converter? the pro mini doesn't have a usb port so it requires a serial convert which is why I am confused. Are you sure its a pro mini? If so, I assume the device signature…
  • clem57
    clem57 over 10 years ago

    Please edit this and move to Arduino if you want answers. This area applies only to software. Also mark as question. Thanks.

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • screamingtiger
    screamingtiger over 10 years ago

    are you using a FDTI serial converter?  the pro mini doesn't have a usb port so it requires a serial convert which is why I am confused.  Are you sure its a pro mini?

     

    If so, I assume the device signature error is a windows error when you plug in the USB?   Do you get this error without the ATTIny85 being hooked up?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gub11
    gub11 over 10 years ago in reply to screamingtiger

    i am using an FTDI cable yes.  I only get the error when i am programming to the attiny with the arduino as an isp.  I can program my arduino pro mini over FTDI cable perfectly, but when i make the connection from the arduino to the attiny85 via breadboard, and try to upload to the tiny, i get a device signature error 0x0000000 while uploading to the tiny, which stops the upload.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gub11
    gub11 over 10 years ago in reply to gub11

    also i made a new post in a more appropratie forum section, http://www.element14.com/community/message/159893/l/programming-attiny85-with-arduino-pro-mini#159893 , please reply there