EAGLE User Support (English) Off board connections
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 314 views
  • Users 0 members are here
Related

Off board connections

autodeskguest
autodeskguest over 18 years ago

I am trying to create a device for a connector that connects  panel

switches to a circuit board.

 

In this case it is a 5 pin connector. I need the device to have 10 pins

so I can represent the connection in the schematic, but only 5 pins in

the package for the pads.

 

I tried to do the symbol with 10 pins and 5 set to NC, but I can not add

the symbol to the package without getting an error about the number of

pins not matching.

 

How do I handle this?

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 18 years ago

    John Giddy wrote:

    DB wrote:

    I am trying to create a device for a connector that connects  panel

    switches to a circuit board.

     

    In this case it is a 5 pin connector. I need the device to have 10

    pins so I can represent the connection in the schematic, but only 5

    pins in the package for the pads.

     

    I tried to do the symbol with 10 pins and 5 set to NC, but I can not

    add the symbol to the package without getting an error about the

    number of pins not matching.

     

    How do I handle this?

     

    I am a bit confused. Why do you need 10 pins for the schematic ?

    Is it to show both the plug and the socket, so you can show the panel

    switches on the schematic ?

    If so, the plug and the socket are separate components and would need

    separate devices in the library.

    AFAIK, you cannot have a device with more pins than pads. A device with

    more pads than pins is OK.

    John G.

     

    That is correct. I need to show the plug and the socket in the

    schematic, but only want pads for the pins that are actually on the board.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 18 years ago

    John Giddy wrote:

    DB wrote:

    I am trying to create a device for a connector that connects  panel

    switches to a circuit board.

     

    In this case it is a 5 pin connector. I need the device to have 10

    pins so I can represent the connection in the schematic, but only 5

    pins in the package for the pads.

     

    I tried to do the symbol with 10 pins and 5 set to NC, but I can not

    add the symbol to the package without getting an error about the

    number of pins not matching.

     

    How do I handle this?

     

    I am a bit confused. Why do you need 10 pins for the schematic ?

    Is it to show both the plug and the socket, so you can show the panel

    switches on the schematic ?

    If so, the plug and the socket are separate components and would need

    separate devices in the library.

    AFAIK, you cannot have a device with more pins than pads. A device with

    more pads than pins is OK.

    John G.

     

    That is correct. I need to show the plug and the socket in the

    schematic, but only want pads for the pins that are actually on the board.