EAGLE User Support (English) Off board connections
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 314 views
  • Users 0 members are here
Related

Off board connections

autodeskguest
autodeskguest over 18 years ago

I am trying to create a device for a connector that connects  panel

switches to a circuit board.

 

In this case it is a 5 pin connector. I need the device to have 10 pins

so I can represent the connection in the schematic, but only 5 pins in

the package for the pads.

 

I tried to do the symbol with 10 pins and 5 set to NC, but I can not add

the symbol to the package without getting an error about the number of

pins not matching.

 

How do I handle this?

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 18 years ago

    DB wrote:

     

    John Giddy wrote:

    DB wrote:

    I am trying to create a device for a connector that connects  panel

    switches to a circuit board.

     

    In this case it is a 5 pin connector. I need the device to have 10

    pins so I can represent the connection in the schematic, but only 5

    pins in the package for the pads.

     

    I tried to do the symbol with 10 pins and 5 set to NC, but I can not

    add the symbol to the package without getting an error about the

    number of pins not matching.

     

    How do I handle this?

     

    I am a bit confused. Why do you need 10 pins for the schematic ?

    Is it to show both the plug and the socket, so you can show the panel

    switches on the schematic ?

    If so, the plug and the socket are separate components and would need

    separate devices in the library.

    AFAIK, you cannot have a device with more pins than pads. A device with

    more pads than pins is OK.

    John G.

     

    That is correct. I need to show the plug and the socket in the

    schematic, but only want pads for the pins that are actually on the board.

     

    Then use lines and not pins for the 5 extra connections on the schematic

    symbol. Play with the line width and length until you get something that

    looks like a pin, but isn't.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 18 years ago

    DB wrote:

     

    John Giddy wrote:

    DB wrote:

    I am trying to create a device for a connector that connects  panel

    switches to a circuit board.

     

    In this case it is a 5 pin connector. I need the device to have 10

    pins so I can represent the connection in the schematic, but only 5

    pins in the package for the pads.

     

    I tried to do the symbol with 10 pins and 5 set to NC, but I can not

    add the symbol to the package without getting an error about the

    number of pins not matching.

     

    How do I handle this?

     

    I am a bit confused. Why do you need 10 pins for the schematic ?

    Is it to show both the plug and the socket, so you can show the panel

    switches on the schematic ?

    If so, the plug and the socket are separate components and would need

    separate devices in the library.

    AFAIK, you cannot have a device with more pins than pads. A device with

    more pads than pins is OK.

    John G.

     

    That is correct. I need to show the plug and the socket in the

    schematic, but only want pads for the pins that are actually on the board.

     

    Then use lines and not pins for the 5 extra connections on the schematic

    symbol. Play with the line width and length until you get something that

    looks like a pin, but isn't.