EAGLE User Support (English) Restring Tolerance Compliance
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
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 423 views
  • Users 0 members are here
Related

Restring Tolerance Compliance

autodeskguest
autodeskguest over 17 years ago

I've been spending the better part of today wasting tons of my company's

money trying to save a buck - it's not making much sense for this

one-time, but I am also hoping this investment will increase my

understanding and either find me a more cost-effective board house or

give me the ability to better test my boards against the various houses

to see who is cheaper in each case.

 

On to the real problem at hand.  I've perused the board and found a few

complaints about the DRC's insistence on CHANGING restrings (annular

ring - as it SHOULD be called because I never stringed anything in the

first place in order to need to REstring it!).  Apparently the DRC even

does this if you have NOT set your pads in your libraries to AUTO.  Even

more dumber.  All this being really bad, to add insult to injury I

really do not CARE what percentage of annular ring I have aorund my

pads, every board house I've look at simply cares about the differential

diameter.  It wouldn't matter to them if I had a via the diameter of a

human hair or one the size of the Himalayans - they want one thing: a

specified amount of diameter LARGER than the drill.  It's not a

percentage, its a hard and fast number.  Why can't EAGLE accept a

percentage, a calculation, or a hard-and-fast value??

 

Suggestion for change?!

 

-Jon

 

  • Sign in to reply
  • Cancel
Parents
  • WestfW
    WestfW over 17 years ago

    Robert Johnson wrote:

     

    Then set the minimum restring to the 'differential diameter' and percentage

    to 0%, for example, 6mil min and 0% generates an annular ring 12mil larger

    than the drill diameter in all cases, unless a larger diameter was set in

    the library device.

     

     

    I had some designs where I "gave up" and modified just the min/max

    restring instead of percentages and found it much easier as well.

     

    BillW

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • WestfW
    WestfW over 17 years ago

    Robert Johnson wrote:

     

    Then set the minimum restring to the 'differential diameter' and percentage

    to 0%, for example, 6mil min and 0% generates an annular ring 12mil larger

    than the drill diameter in all cases, unless a larger diameter was set in

    the library device.

     

     

    I had some designs where I "gave up" and modified just the min/max

    restring instead of percentages and found it much easier as well.

     

    BillW

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 17 years ago in reply to WestfW

    Rob and Bill:

    I came to that conclusion myself.  It sounds like EAGLE and Microsoft

    have similar programming mentalities.  Write the program any old way and

    make the user find work-arounds.

     

    I guess the reason for my post was to see if I understood what was going

    on correctly, and if I did to complain about it profusely.  IMHO this is

    a really poor way of handling annular rings, and I will explain:

     

    1)The DRC is a design rule CHECKER... I don't see anything in that title

    that suggests CHANGING anything.  If it's to change my annular rings,

    (or RESTrings, thanks Richard) then why not also change my routing

    choices, or me board dimensions, or move my components so they match

    some setting.

     

    2)What if I want one part to be different from another?  If it worked

    the way I think it should I simply update one library and voila, my new

    annular ring sizes are changed only how and where I want them to.

     

    3)What in the world is the point in defining pad size in a library if

    the DRC is going to handle it as it sees fit?  Why wouldn't I just name

    an X,Y point for the center and a diameter for the hole in the library

    leaving the diameter for the ring a non-option here because the DRC is

    going to change it anyway!

     

    4)Has anyone EVER used this feature in the DRC to an ADVANTAGE?  Or are

    we all cussing at it and figuring out how to work around it so our

    pads/via and their annular rings are showing up as we created them to?

     

    May I suggest: get rid of the percentage option.  This is the one thing

    that is implementing a change on this page.  Change the Max/Min to

    CHECKS only!  (gee, golly, since the DRC is a CHECKER after all, maybe

    it should just CHECK things and report!)

     

     

    Bill Westfield wrote:

    Robert Johnson wrote:

     

    Then set the minimum restring to the 'differential diameter' and

    percentage

    to 0%, for example, 6mil min and 0% generates an annular ring 12mil

    larger

    than the drill diameter in all cases, unless a larger diameter was set in

    the library device.

     

    I had some designs where I "gave up" and modified just the min/max

    restring instead of percentages and found it much easier as well.

     

    BillW