EAGLE User Support (English) Changing Track Thickness and Filling GND Track
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 217 views
  • Users 0 members are here
Related

Changing Track Thickness and Filling GND Track

autodeskguest
autodeskguest over 18 years ago

I am using the unregistered version of eagle.I want to increase the Track

Width.How do I do it.Also is it possible to fill the unused part of the

board with a GND track

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    Mahesh wrote:

    I am using the unregistered version of eagle.I want to increase the Track

    Width.How do I do it.

    Click on Change/width and choose the width.  You can also choose the

    track width as you hand route a track.  You can also type the command

       change width 5       if the grid is mm,  this will be 5 mm

                            if the grid is mil, this will be 5 mil

     

     

    Also is it possible to fill the unused part of the

    board with a GND track.

    This is also known as a copper pour.  Use the POLYGON command to draw a

    rectangle around the entire board.  I find that a 16 mil (~0.4mm) width

    works well.  Name the polygon GND, and then click on RATSNEST (it's an

    "X" with dots on the tips of the "X"), or type "ratsnest".

     

    AFAIK, all of this info is in the EAGLE tutorial.

     

    -Dave Pollum