Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) hey, i made a circular board layout in eagle. i upgraded to eagle standard, so the board can be up to 160cm2, my circle has a radius of 2480mil and all components are inside (0 0). the layout is finished, but i decided to change 1 last part, now suddenly
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 818 views
  • Users 0 members are here
  • eagle cannot perform the requested function
Related

hey, i made a circular board layout in eagle. i upgraded to eagle standard, so the board can be up to 160cm2, my circle has a radius of 2480mil and all components are inside (0 0). the layout is finished, but i decided to change 1 last part, now suddenly

broccoli
broccoli over 7 years ago

hey, i made a circular board layout in eagle. i upgraded to eagle standard, so the board can be up to 160cm2, my circle has a radius of 2480mil and all components are inside (0 0). the layout is finished, but i decided to change 1 last part, now suddenly the message 'Eagle cannot perform the requested function. Some objects extend outside the allowed board area' turns up. i cant move that last part onto the board. can someone tell me whats going wrong there? thanks.

Attachments:
image
  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago

    On 15/12/2018 12:41 AM, daniela hüsser wrote:

    hey, i made a circular board layout in eagle. i upgraded to eagle standard, so the board can be up to 160cm2, my circle has a radius of 2480mil and all components are inside (0 0). the layout is finished, but i decided to change 1 last part, now suddenly the message 'Eagle cannot perform the requested function. Some objects extend outside the allowed board area' turns up. i cant move that last part onto the board. can someone tell me whats going wrong there? thanks.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/269603

     

    Attachments:

    eagle.png

     

     

     

    Hi

     

    There is a setting for the dimensions of your permitted 160cm2.

     

    Check that your circle fits within it. The setting can make the 160cm2

    tall and skinny down to wide and flat.

     

    You may need to make yours 40mm x 40 mm .

     

    HTH

    Warren

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 7 years ago

    Is it possible there is something on a hidden layer which you cannot currently see? If you do a zoom to fit does it zoom to fit just the board and the final component or does it zoom out some more? Without seeing the actual board it's hard to tell what the issue is but these would be the first things to check.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago

    I haven't seen this issue since I have an unlimited version of Eagle, but if you really need a work-around...

    If you have a part with the same footprint already on the card, you could duplicate it. This will disconnect the schematic from the layout, so you will need to add a corresponding part with the same name to the schematic before connecting the part to the circuit.