EAGLE User Support (English) rebel LED package
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
  • Replies 10 replies
  • Subscribers 178 subscribers
  • Views 711 views
  • Users 0 members are here
Related

rebel LED package

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I'm already two days busy trying to design the package for a Luxeon Rebel

LED (see attached files). It is very difficult and time-consuming to design.

I'm drawing each pad as a polygon now. Is this the right way or does someone

have a faster and simpler method?

 

Best regards,

Mark

 

 

 

 

 

 

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    M.Klaassens wrote:

    Dear Chuck

     

    I followed your instructions. And added a small example. Is this the right

    way to do it? Aren't the via's filled with solder during the reflow process?

     

    Do you also have any idea why it's possible that the via's in the board are

    bigger than those in the package design??

     

    Thanks

    Mark

     

     

    "Chuck Huber" <chuck.huber@dukepro.com> schreef in bericht

    news:fpcb7u$m9$1@cheetah.cadsoft.de...

    M.Klaassens wrote:

    Hi,

     

    I designed the footprint, as attached. But now I want to connect all

    via's to the V(ia)-pin. Anyone any suggestions?

    I ran across this problem with a PCB mounted fuse clip designed to accept

    one end of a cylindrical fuse.  The clip has two pins on the same net.

     

    At present, there is no way to connect multiple plated through-holes to

    the same pin in the schematic - it's always a one-to-one relationship

    between pads/holes in the package and pins in the schematic.

     

    To work around this, I created the part with some copper on the bFill

    (layer 101) layer and included that layer with the top copper in the .cam

    file.  This avoids all the DRC errors produced when you have bottom copper

    bridging both pins.

     

    In my application, I have a 70 to 90 amp impulse lasting about 2.5 to 3.0

    us going through the part.  I wanted to make sure that all the holes were

    connected to copper to reduce inductive and IR impedence losses.

    Basically, the current traveling along the trace had to turn "up" to get

    to the clip.  This amounts to a 1/4 turn inductor.

     

     

    In the case of the Rebel LED package, you may want add a polygon on the

    tFill (101) and bFill (102) layers that surrounds all the vias.  Be sure

    to modify you CAM file to include tFill with the top copper and bFill with

    bottom copper.  On the schematic, you can have one pin connected to one of

    the vias.

     

    When you produce the gerber files, double check the top and bottom copper

    layers to make sure the fill has been included.

     

    While it's not the ideal approach, it is a decent workaround that will get

    you copper where you need it.

     

    Hope this helps,

     

        - Chuck

     

     

    If the vias are to help extract heat from the package, filling with

    solder will be better than filling with air or solder resist.

    John G.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    M.Klaassens wrote:

    Dear Chuck

     

    I followed your instructions. And added a small example. Is this the right

    way to do it? Aren't the via's filled with solder during the reflow process?

     

    Do you also have any idea why it's possible that the via's in the board are

    bigger than those in the package design??

     

    Thanks

    Mark

     

     

    "Chuck Huber" <chuck.huber@dukepro.com> schreef in bericht

    news:fpcb7u$m9$1@cheetah.cadsoft.de...

    M.Klaassens wrote:

    Hi,

     

    I designed the footprint, as attached. But now I want to connect all

    via's to the V(ia)-pin. Anyone any suggestions?

    I ran across this problem with a PCB mounted fuse clip designed to accept

    one end of a cylindrical fuse.  The clip has two pins on the same net.

     

    At present, there is no way to connect multiple plated through-holes to

    the same pin in the schematic - it's always a one-to-one relationship

    between pads/holes in the package and pins in the schematic.

     

    To work around this, I created the part with some copper on the bFill

    (layer 101) layer and included that layer with the top copper in the .cam

    file.  This avoids all the DRC errors produced when you have bottom copper

    bridging both pins.

     

    In my application, I have a 70 to 90 amp impulse lasting about 2.5 to 3.0

    us going through the part.  I wanted to make sure that all the holes were

    connected to copper to reduce inductive and IR impedence losses.

    Basically, the current traveling along the trace had to turn "up" to get

    to the clip.  This amounts to a 1/4 turn inductor.

     

     

    In the case of the Rebel LED package, you may want add a polygon on the

    tFill (101) and bFill (102) layers that surrounds all the vias.  Be sure

    to modify you CAM file to include tFill with the top copper and bFill with

    bottom copper.  On the schematic, you can have one pin connected to one of

    the vias.

     

    When you produce the gerber files, double check the top and bottom copper

    layers to make sure the fill has been included.

     

    While it's not the ideal approach, it is a decent workaround that will get

    you copper where you need it.

     

    Hope this helps,

     

        - Chuck

     

     

    If the vias are to help extract heat from the package, filling with

    solder will be better than filling with air or solder resist.

    John G.