EAGLE User Support (English) rebel LED package
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
  • Replies 10 replies
  • Subscribers 178 subscribers
  • Views 710 views
  • Users 0 members are here
Related

rebel LED package

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I'm already two days busy trying to design the package for a Luxeon Rebel

LED (see attached files). It is very difficult and time-consuming to design.

I'm drawing each pad as a polygon now. Is this the right way or does someone

have a faster and simpler method?

 

Best regards,

Mark

 

 

 

 

 

 

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Chuck Huber wrote:

    M.Klaassens wrote:

    Hi,

     

    I designed the footprint, as attached. But now I want to connect all

    via's to the V(ia)-pin. Anyone any suggestions?

     

    I ran across this problem with a PCB mounted fuse clip designed to

    accept one end of a cylindrical fuse.  The clip has two pins on the

    same net.

    ...

     

    Another way to deal with this situation is to simply put multiple pins in

    the schematic Symbol, each pin being connected to one pad in the Device.  In

    the schematic you simply connect your Net to both pins.  This produces

    exactly what you want without any additional copper layers not checked by

    DRC, and without any DRC errors.

     

    --

    Bert Menkveld

     

     

    At present, there is no way to connect multiple plated through-holes

    to the same pin in the schematic - it's always a one-to-one

    relationship between pads/holes in the package and pins in the

    schematic.

    To work around this, I created the part with some copper on the bFill

    (layer 101) layer and included that layer with the top copper in the

    .cam file.  This avoids all the DRC errors produced when you have

    bottom copper bridging both pins.

     

    In my application, I have a 70 to 90 amp impulse lasting about 2.5 to

    3.0 us going through the part.  I wanted to make sure that all the

    holes were connected to copper to reduce inductive and IR impedence

    losses. Basically, the current traveling along the trace had to turn

    "up" to get to the clip.  This amounts to a 1/4 turn inductor.

     

     

    In the case of the Rebel LED package, you may want add a polygon on

    the tFill (101) and bFill (102) layers that surrounds all the vias. Be

    sure to modify you CAM file to include tFill with the top copper

    and bFill with bottom copper.  On the schematic, you can have one pin

    connected to one of the vias.

     

    When you produce the gerber files, double check the top and bottom

    copper layers to make sure the fill has been included.

     

    While it's not the ideal approach, it is a decent workaround that will

    get you copper where you need it.

     

    Hope this helps,

     

        - Chuck

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Chuck Huber wrote:

    M.Klaassens wrote:

    Hi,

     

    I designed the footprint, as attached. But now I want to connect all

    via's to the V(ia)-pin. Anyone any suggestions?

     

    I ran across this problem with a PCB mounted fuse clip designed to

    accept one end of a cylindrical fuse.  The clip has two pins on the

    same net.

    ...

     

    Another way to deal with this situation is to simply put multiple pins in

    the schematic Symbol, each pin being connected to one pad in the Device.  In

    the schematic you simply connect your Net to both pins.  This produces

    exactly what you want without any additional copper layers not checked by

    DRC, and without any DRC errors.

     

    --

    Bert Menkveld

     

     

    At present, there is no way to connect multiple plated through-holes

    to the same pin in the schematic - it's always a one-to-one

    relationship between pads/holes in the package and pins in the

    schematic.

    To work around this, I created the part with some copper on the bFill

    (layer 101) layer and included that layer with the top copper in the

    .cam file.  This avoids all the DRC errors produced when you have

    bottom copper bridging both pins.

     

    In my application, I have a 70 to 90 amp impulse lasting about 2.5 to

    3.0 us going through the part.  I wanted to make sure that all the

    holes were connected to copper to reduce inductive and IR impedence

    losses. Basically, the current traveling along the trace had to turn

    "up" to get to the clip.  This amounts to a 1/4 turn inductor.

     

     

    In the case of the Rebel LED package, you may want add a polygon on

    the tFill (101) and bFill (102) layers that surrounds all the vias. Be

    sure to modify you CAM file to include tFill with the top copper

    and bFill with bottom copper.  On the schematic, you can have one pin

    connected to one of the vias.

     

    When you produce the gerber files, double check the top and bottom

    copper layers to make sure the fill has been included.

     

    While it's not the ideal approach, it is a decent workaround that will

    get you copper where you need it.

     

    Hope this helps,

     

        - Chuck