Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) 274X supports polygon shapes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 934 views
  • Users 0 members are here
Related

274X supports polygon shapes

cgantenbein
cgantenbein over 7 years ago

Eagle’s 274X output is vector based.  274X supports polygon shapes (outlines) filled solid as a copper pour.  Eagle’s 274X is not utilizing this available option causing huge files.

Is there a way to remedy?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 7 years ago

    On 3/1/2019 2:45, Chris Gantenbein wrote:

    Eagle’s 274X output is vector based.  274X supports polygon shapes (outlines) filled solid as a copper pour.  Eagle’s 274X is not utilizing this available option causing huge files.

    Is there a way to remedy?

     

    I have been looking into this, but never got to the end of it. I have

    this gerber ULP that I made years ago and really wanted to check if I

    could use polygon fill to both get rid of the fixed wire fill overlap

    issue (causing rounding issues at certain precision) and to get the

    filesize down. I gave it up at the time, but I still think it is doable.

     

    I think (not confirmed) that Cadsoft/Autodesk stays away from it because

    there may be both gerber viewers and routing gear out there that can't

    handle it correctly/consistent, but I still think it should be an option

    in the DRC Layers setup. It would make Eagle draw fills much faster on

    screen too.

     

    Gerber X2 may be a better target for this function, as you don't have to

    support older gear and software.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 7 years ago

    On 3/1/2019 2:45, Chris Gantenbein wrote:

    Eagle’s 274X output is vector based.  274X supports polygon shapes (outlines) filled solid as a copper pour.  Eagle’s 274X is not utilizing this available option causing huge files.

    Is there a way to remedy?

     

    I have been looking into this, but never got to the end of it. I have

    this gerber ULP that I made years ago and really wanted to check if I

    could use polygon fill to both get rid of the fixed wire fill overlap

    issue (causing rounding issues at certain precision) and to get the

    filesize down. I gave it up at the time, but I still think it is doable.

     

    I think (not confirmed) that Cadsoft/Autodesk stays away from it because

    there may be both gerber viewers and routing gear out there that can't

    handle it correctly/consistent, but I still think it should be an option

    in the DRC Layers setup. It would make Eagle draw fills much faster on

    screen too.

     

    Gerber X2 may be a better target for this function, as you don't have to

    support older gear and software.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • cgantenbein
    0 cgantenbein over 7 years ago in reply to autodeskguest

    We are very aware of how line width affects the database. However, we need to use a particular min. line width to achieve ground fill around dense via locations. This is a large 26 layer board with multiple ground layers (single stripline stackup). Consequently, fab processing time and effort is becoming inordinate trying to handle the 200M+ vectorized Gerbers. The question I posed actually came from our fab suggesting a way to solve this problem.

     

    Searching. Is there a run Gerber command line option with parameters/flags we could set differently from the default mode in order to help our situation, such as mentioned above, turning on polygon fill? Or, other command line options that might help?