EAGLE User Support (English) Eagle 4.0 linux 64bit
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 393 views
  • Users 0 members are here
Related

Eagle 4.0 linux 64bit

autodeskguest
autodeskguest over 17 years ago

I just reinstalled my old Eagle 4.0 professional on SUSE 10.3 64 bit.

I can open the program. when I try to edit library to make a new symbol, it

works only until I try to add a pin. then it crashes with a message:

Floating point exception. I didn't try to do anything else yet.

there is no point if I can't create devices I need.

The same version worked fine before on 32 bit SUSE 10.2.

Is it a Linux  or Eagle problem?

Regards

Marek Kiela

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    kielam@mcmaster.ca schrieb:

    I just reinstalled my old Eagle 4.0 professional on SUSE 10.3 64 bit.

    I can open the program. when I try to edit library to make a new symbol, it

    works only until I try to add a pin. then it crashes with a message:

    Floating point exception. I didn't try to do anything else yet.

    there is no point if I can't create devices I need.

    The same version worked fine before on 32 bit SUSE 10.2.

    Is it a Linux  or Eagle problem?

    Regards

    Marek Kiela

     

    What's the EAGLE version you are working with? Is it 4.09r2, the

    latest 4.0, or an earlier one? If it is not 4.09r2, please download

    and try it.

    ftp:/ftp.cadsoft.de/pub/program/4.0

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm