Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Same net but different net class with Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 189 subscribers
  • Views 1995 views
  • Users 0 members are here
  • power nets
  • editing traces
  • trace-width
  • pcb trace
Related

Same net but different net class with Eagle

fabboco
fabboco over 7 years ago

I have a trace which powers an external device and with a large size because it carries a relative high current (more than 1A).

Along this trace I have a small value resistor to monitor the flowing current.

The resistor is connected to an ADC to measure current. The traces between the resistor and the ADC can be smaller than the power traces because not much current flows there.

I am not able to use two different net classes for the power trace and for the ADC traces. A soon as I change the class of the power trace, the sensors traces get the same net class and viceversa.

I have also tried to put a 0 ohm resistors along the sensor traces but this doesn't help neither.

Can anyone help me with this issue?

Thx

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 7 years ago

    Fabrizio,

     

    Look in the shorts.lbr file.  It consists of two SMD pads that overlap. 

    By putting a short in series with your smaller resistor, it forms two

    different nets.  The net between the short and the resistor could be

    assigned a different class allowing the narrower trace.  I can send a

    shorts library to you.  Olin Lathrop is the original author, and I've

    added a couple of my own.  Olin has published it on the Internet, which

    is where I found it years ago.

     

    My primary use of shorts is to connect different grounds together.  i.e.

    I'll have a DGND, AGND, and HVGND representing grounds used in different

    areas of a design (digital, analog, and high voltage).  In the end, all

    these grounds need to be connected together.  I'll connect DGND to GND

    through a short, then AGND to GND, and HVGND to GND.  Just plain old GND

    will be routed back to the battery, or power supply or whatever.

     

    Of course, you could use the narrower trace just as you have it now. 

    When you do the DRC, you can approve the error it generates and it'll

    never bother you again... at least until you move it.

     

    HTH,

        - Chuck

     

     

    On 4/16/19 02:38, Fabrizio Boco wrote:

    I have a trace which powers an external device and with a large size because it carries a relative high current (more than 1A).

    Along this trace I have a small value resistor to monitor the flowing current.

    The resistor is connected to an ADC to measure current. The traces between the resistor and the ADC can be smaller than the power traces because not much current flows there.

    I am not able to use two different net classes for the power trace and for the ADC traces. A soon as I change the class of the power trace, the sensors traces get the same net class and viceversa.

    I have also tried to put a 0 ohm resistors along the sensor traces but this doesn't help neither.

    Can anyone help me with this issue?

    Thx

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/274385

     

     

    Attachments:
    5861.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fabboco
    0 fabboco over 7 years ago in reply to dukepro

    Hi Chuck,

    Thank you very much. That is exactly what I was looking for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fabboco
    0 fabboco over 7 years ago in reply to dukepro

    Hi Chuck,

    Thank you very much. That is exactly what I was looking for.