Hi guys!
I am in a bit of a piccle here. Somehow the install for Eagle 4.16r2 fails
on Windows XP x64. Letting it unpack and trying the setup.exe directly
gives an error saying "The image file setup.exe is valid, but is for a
machine type other than the current machine type."
Normally the emulation in x64 should allow regular XP compativle programs to
run but something is blocking this setup.
I tried 4.16r1 but I get the same error.
Copying the old installation of 4.16r1 from regular XP into the x64
installation works so it appears that the previous software itself has no
problems running. Just the installer.
What gives? No x64 support?
Kyrre