Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 5.10.0 libraries and Win10
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1484 views
  • Users 0 members are here
Related

Eagle 5.10.0 libraries and Win10

davebullockmbe
davebullockmbe over 7 years ago

Dear Sir,

Has anyone else reported issues with older versions of EAGLE when migrating to Win10?

I have been using EAGLE for over 20 years and my licence allowed me to get as far as Ver5.10.0.

I have been running it trouble free on Win7 since this version of Windows arrived. I have now migrated to a brand new installation of Windows 10 and am getting 'Data errors' in libraries as soon as I click 'add new part'.

There are maybe 6 or seven libraries that flag up this error which is really annoying.

However I have a Microsoft 'Surface' running Win10 and EAGLE 5.10.0 and this doesn't exhibit the same behaviour.

So thinking the new installation had corrupted libraries, I copied the 'suspect' libraries from the 'surface' to my new installation but the 'Data error' message persists. (so replacing the libraries doesn't cure the fault).

Any anecdotal information or advice please?

Thanks

Dave

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to davebullockmbe

    Am 30.08.2019 um 16:28 schrieb Dave Bullock MBE:

    HI thanks for your swift replies,

    Would file privilege issues just affect 6 libraries out of all the EAGLE libraries?

    As I said it's only libraries like (for instance) 74xx-little-us.lbr and con-avx.lbr that throw up this error message and the rest of the libraries load without problem when I click 'add new part'.

    EAGLE then works fine as long as I don't try to access these faulty? libraries.

    However on my Win10 laptop the same installation works faultlessly with the same version of EAGLE.

    Finally deleting the faulty libraries and copying them across from the working version on my laptop delivers the same errors on the newly copied libraries.

    It's as though the main EAGLE program is somehow not recognising the libraries rather than them being faulty.

     

    I guess I could reinstall EAGLE 5.10.0 or as Morten suggests try the last release?

    It's very weird :-o

    Dave

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/280278

     

     

    Could it be that those files were modified?

    If you need to modify libraries don't do it in the originals, but save

    them in your own libraries.

     

    Download eagle 5.12

    ftp://ftp.cadsoft.de/eagle/program/

     

    Imho versions lower than 6.6 are not available on autodesk server.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • davebullockmbe
    0 davebullockmbe over 7 years ago

    HI thanks for your swift replies,

    Would file privilege issues just affect 6 libraries out of all the EAGLE libraries?

    As I said it's only libraries like (for instance) 74xx-little-us.lbr and con-avx.lbr that throw up this error message and the rest of the libraries load without problem when I click 'add new part'.

    EAGLE then works fine as long as I don't try to access these faulty? libraries.

    However on my Win10 laptop the same installation works faultlessly with the same version of EAGLE.

    Finally deleting the faulty libraries and copying them across from the working version on my laptop delivers the same errors on the newly copied libraries.

    It's as though the main EAGLE program is somehow not recognising the libraries rather than them being faulty.

     

    I guess I could reinstall EAGLE 5.10.0 or as Morten suggests try the last release?

    It's very weird :-o

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to autodeskguest

    Am 30.08.2019 um 12:51 schrieb Morten Leikvoll:

    On 8/30/2019 9:35, Dave Bullock MBE wrote:

    Dear Sir,

    Has anyone else reported issues with older versions of EAGLE when

    migrating to Win10?

    I have been using EAGLE for over 20 years and my licence allowed me to

    get as far as Ver5.10.0.

    I have been running it trouble free on Win7 since this version of

    Windows arrived. I have now migrated to a brand new installation of

    Windows 10 and am getting 'Data errors' in libraries as soon as I

    click 'add new part'.

    There are maybe 6 or seven libraries that flag up this error which is

    really annoying.

    However I have a Microsoft 'Surface' running Win10 and EAGLE 5.10.0

    and this doesn't exhibit the same behaviour.

    So thinking the new installation had corrupted libraries, I copied the

    'suspect' libraries from the 'surface' to my new installation but the

    'Data error' message persists. (so replacing the libraries doesn't

    cure the fault).

    Any anecdotal information or advice please?

    Thanks

    Dave

     

    I would immediately suspect some file privilege issues. Make sure the

    installation is in a root folder, and make sure you have full access to

    all files.

     

    Besides Mortens advise upgrade to version 5.12.0. which is

    the latest Vers. 5. It has some advantages and your license allows to

    install it.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago

    On 8/30/2019 9:35, Dave Bullock MBE wrote:

    Dear Sir,

    Has anyone else reported issues with older versions of EAGLE when migrating to Win10?

    I have been using EAGLE for over 20 years and my licence allowed me to get as far as Ver5.10.0.

    I have been running it trouble free on Win7 since this version of Windows arrived. I have now migrated to a brand new installation of Windows 10 and am getting 'Data errors' in libraries as soon as I click 'add new part'.

    There are maybe 6 or seven libraries that flag up this error which is really annoying.

    However I have a Microsoft 'Surface' running Win10 and EAGLE 5.10.0 and this doesn't exhibit the same behaviour.

    So thinking the new installation had corrupted libraries, I copied the 'suspect' libraries from the 'surface' to my new installation but the 'Data error' message persists. (so replacing the libraries doesn't cure the fault).

    Any anecdotal information or advice please?

    Thanks

    Dave

     

    I would immediately suspect some file privilege issues. Make sure the

    installation is in a root folder, and make sure you have full access to

    all files.