EAGLE User Support (English) Library: multiple pads per symbol pin
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
  • Replies 2 replies
  • Subscribers 177 subscribers
  • Views 351 views
  • Users 0 members are here
Related

Library: multiple pads per symbol pin

autodeskguest
autodeskguest over 17 years ago

Lots of components have a few internally connected pads, such as this one:

http://www.national.com/pf/LM/LMH6582.html

It has 7 GND, 12 Vee and 12 Vcc pins. It would be very nice to have only

one GND pin in schematic symbol and all of these pads connected together

in PCB layout.

 

Is there any way to do this?

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    circuit wrote:

    Lots of components have a few internally connected pads, such as this

    one: http://www.national.com/pf/LM/LMH6582.html

    It has 7 GND, 12 Vee and 12 Vcc pins. It would be very nice to have

    only one GND pin in schematic symbol and all of these pads connected

    together in PCB layout.

     

    Is there any way to do this?

     

    No, there isn't.  You have to put multiple GND pins in the shematic Symbol

    (you can call them GND@1, GND@2, ..., so they all appear as simply GND in

    the schematic).  You then connect each Symbol pin to a single Package pad.

     

    While you are right that this sometimes produces an awkward looking

    schematic symbol, it does allow you to show all the pad names on the

    schematic.  Very useful when you're probing around a board.  I personally

    hate schematics that hide the power and ground pins.  But obviously some

    other people don't.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Bert Menkveld wrote:

      > No, there isn't.  You have to put multiple GND pins in the shematic

    Symbol

    (you can call them GND@1, GND@2, ..., so they all appear as simply GND in

    the schematic).  You then connect each Symbol pin to a single Package pad.

     

    While you are right that this sometimes produces an awkward looking

    schematic symbol, it does allow you to show all the pad names on the

    schematic.  Very useful when you're probing around a board.  I personally

    hate schematics that hide the power and ground pins.  But obviously some

    other people don't.

     

     

    Oh, that @ thing is new to me. Thanks image