Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Beginner Questions
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1255 views
  • Users 0 members are here
  • circuit board layout
Related

Beginner Questions

perryaire
perryaire over 7 years ago

I recently sent my first circuit board off to OSH Park and the prototypes came back. I made several mistakes that I think any regular user of Eagle software would not make.

  1. First, the titling is nearly invisible. Just font color changes?
  2. Second, the mounting holes appear as dimples in the top layer. Any idea how to get them to be through holes?
  3. Finally, the mounting holes for resisters are much too close together. I can fix that by measuring the the resistors. The library provides 0.1 inch centers.

Thanks in advance for any advice in addressing 1 and 2.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 7 years ago

    For #2, take a look at https://electronics.stackexchange.com/questions/137394/mounting-hole-on-a-pcb . I am assuming you want them to be a GND.

     

    To get the same holes in your eagle project go to your schematic and click on add (or type add in the text box and hit enter). Now to go the holes library, then you see there is a MOUNT-PAD-ROUND and a MOUNT-PAD-SQUARE library. These are the library's you are looking for. In the schematic you can connect the pad to a signal, which is mostly used to connect to ground (not sure about this). And yes on the blue PCB's they are also functioning as via's probably because the screws are connected to ground.

    The holes in your mounting hole is probably there so more current can flow through. To get these holes also in your eagle project you probably need to make your own library for that. The golden finish on the mounting hole is there because it is considered as a via or regular hole.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago

    For #2, take a look at https://electronics.stackexchange.com/questions/137394/mounting-hole-on-a-pcb . I am assuming you want them to be a GND.

     

    To get the same holes in your eagle project go to your schematic and click on add (or type add in the text box and hit enter). Now to go the holes library, then you see there is a MOUNT-PAD-ROUND and a MOUNT-PAD-SQUARE library. These are the library's you are looking for. In the schematic you can connect the pad to a signal, which is mostly used to connect to ground (not sure about this). And yes on the blue PCB's they are also functioning as via's probably because the screws are connected to ground.

    The holes in your mounting hole is probably there so more current can flow through. To get these holes also in your eagle project you probably need to make your own library for that. The golden finish on the mounting hole is there because it is considered as a via or regular hole.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 7 years ago in reply to clem57

    If you would like to learn more, read https://www.lucidar.me/en/eagle/adding-mounting-holes-to-a-PCB/ ...