EAGLE User Support (English) Re: Slotted pads for library device
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
  • Replies 0 replies
  • Subscribers 177 subscribers
  • Views 109 views
  • Users 0 members are here
Related

Re: Slotted pads for library device

autodeskguest
autodeskguest over 17 years ago

drew keller wrote:

I am mounting a PCB to a transformer that has quick terminals on it. So

I am trying to create a library part that has slotted through hole pads....

 

I created the slotted pads in the package by drawing thick WIREs in the

pads layer and thin WIREs in the milling layer. But when I try to bring

the package into the device definition, there is an error that says

there are not enough pads to match my symbol.

 

Maybe there is a better way to do this.

 

Thanks.

-drew

 

You never created any actual pads that EAGLE recognizes.  EAGLE makes a

distinction b/t places where your are just defining metal and if a

defined area of metal is a pad meant for electrical connection in a

netlist.

 

What you should probably do is:

 

-Create the slot in the Milling(46) layer.

-Add an SMD pad to either the Top(1) or Bottom(16) layer.

-Draw a polygon of the same shape as the SMD pad, and place it on the

opposite layer.

-When you CAM-up your .brd file add an extra section, call it MILLING,

set the extension to .mll, select the Milling(46) layer and process the

entire job.

-Tell your board house that the .mll file has information on milling

that needs to be done before metallization.