Okay, so at least SOMETHING is consistent!... THE PROBLEM KEEPS COMING BACK!
I did ALL of this in 5 minutes without opening or closing any new
windows: I opened a new library, created the one and only part I
needed. I opened a new schematic, did a "use -*" then a "use [my
library.lbr]" so my only library of choice after an "add" is the one I
just made. I added my one part 12 times. I did a "board" command and
arranged the headers. I decided the silks didn't represent the size of
the headers properly with the ejectors/latches and increased the silks
in the library. I then did an "update all" and nothing changed.
WTF?!?!? WTFF?!?!?
I then deleted them all from the schematic. I simply typed "add" and
added the 12 headers AGAIN into the schematic. When I looked at the
board it had all 12 headers with their latest versions. WTFFFFFF?!?!?! F
I'm mad...
-jh