EAGLE User Support (English) Mac two finger scrolling
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 302 views
  • Users 0 members are here
Related

Mac two finger scrolling

autodeskguest
autodeskguest over 17 years ago

Mac version 4.92.8

When "two finger scrolling" is enabled in the trackpad preferences of

my Mac Book Pro, Eagle interprets this as "two finger zooming" instead

of scrolling. It probably should match the behavior intended, as other

programs do.

 

 

  • Sign in to reply
  • Cancel
  • kcadsoft
    kcadsoft over 17 years ago

    On 04/18/08 14:38, Joe wrote:

    Mac version 4.92.8

     

    This message should have gone into eagle.betatest image

     

    When "two finger scrolling" is enabled in the trackpad preferences of my

    Mac Book Pro, Eagle interprets this as "two finger zooming" instead of

    scrolling. It probably should match the behavior intended, as other

    programs do.

     

    EAGLE has no concept of "two finger" actions. It can only react

    on what Qt 4 delivers (I don't know if Qt 4.4 already supports

    these "two finger" gestures - EAGLE 4.02.8 is based on Qt 4.3.3).

     

    Maybe "two finger scrolling" is actually mapped to a scroll wheel

    action. In that case you can set the scroll factor to 0 in the

    Control Panel under "Options/User interface", and then EAGLE will

    scroll instead of zoom.

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Hofmark 2                               Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    On 2008-04-18 08:03:10 -0600, Klaus Schmidinger

    <Klaus.Schmidinger@cadsoft.de> said:

     

    On 04/18/08 14:38, Joe wrote:

    Mac version 4.92.8

     

    This message should have gone into eagle.betatest image

     

    When "two finger scrolling" is enabled in the trackpad preferences of

    my Mac Book Pro, Eagle interprets this as "two finger zooming" instead

    of scrolling. It probably should match the behavior intended, as other

    programs do.

     

    EAGLE has no concept of "two finger" actions. It can only react

    on what Qt 4 delivers (I don't know if Qt 4.4 already supports

    these "two finger" gestures - EAGLE 4.02.8 is based on Qt 4.3.3).

     

    Maybe "two finger scrolling" is actually mapped to a scroll wheel

    action. In that case you can set the scroll factor to 0 in the

    Control Panel under "Options/User interface", and then EAGLE will

    scroll instead of zoom.

     

    Klaus Schmidinger

     

    Sorry, didn't realize there was an eagle.betatest.

     

    Setting the zoom factor (not scroll factor) to 0 will cause it not to

    zoom or scroll. That's better than zooming, for me, anyway. It does

    look like "two finger scrolling" is mapped to a scroll wheel event, but

    Eagle chooses to interpret it as a zoom wheel event instead. Calling it

    "Zoom Factor" in the "Options/User Interface" setting indicates that

    this was on purpose. Nothing wrong with that, but it might be good to

    give the option of using "two finger scrolling" and the mouse scroll

    wheel to scroll instead of zoom, which is more common. On my mouse it's

    called a scroll wheel, but in Eagle it zooms.