EAGLE User Support (English) Introduction to BGAs
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
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 231 views
  • Users 0 members are here
Related

Introduction to BGAs

autodeskguest
autodeskguest over 17 years ago

 

Hello,

 

I have been avoiding BGAs until now, but it seems that I

can't do avoid them anymore... I'm having some issues that would

need clarifications though, before I even start experimenting.

 

The BGA I'm considering has following specifications:

     Ball pitch 0.8mm

     Ball diameter 0.4mm

     Ball landing 0.43mm

     Solder mask opening 0.3mm

 

The latter two are somewhat confusing. Does that really

mean that the the diameter of solder mask opening is smaller

than the ball itself, ie, the copper should be partially

covered from edges by the mask? (and follow up if so; "how

that is done?")

 

Then, somehow I don't feel comfortable using very small (0.1mm)

drills, but guess there is no way to avoid those? Or would it

be better to use larger drill and smaller diameter copper

around it?

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Toni Rasan schrieb:

     

    Hello,

     

    I have been avoiding BGAs until now, but it seems that I

    can't do avoid them anymore... I'm having some issues that would

    need clarifications though, before I even start experimenting.

     

    The BGA I'm considering has following specifications:

        Ball pitch 0.8mm

        Ball diameter 0.4mm

        Ball landing 0.43mm

        Solder mask opening 0.3mm

     

    The latter two are somewhat confusing. Does that really

    mean that the the diameter of solder mask opening is smaller

    than the ball itself, ie, the copper should be partially

    covered from edges by the mask? (and follow up if so; "how

    that is done?")

     

     

    How is it done?

    Switch off the automatic generation of the solder stop symbols

    for your SMDs in the Package Editor (CHANGE STOP OFF) and draw

    the solder stop mask manually with a CRICLE. with = 0, in the

    tStop layer.

     

     

     

    Then, somehow I don't feel comfortable using very small (0.1mm)

    drills, but guess there is no way to avoid those? Or would it

    be better to use larger drill and smaller diameter copper

    around it?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Toni Rasan schrieb:

     

    Hello,

     

    I have been avoiding BGAs until now, but it seems that I

    can't do avoid them anymore... I'm having some issues that would

    need clarifications though, before I even start experimenting.

     

    The BGA I'm considering has following specifications:

        Ball pitch 0.8mm

        Ball diameter 0.4mm

        Ball landing 0.43mm

        Solder mask opening 0.3mm

     

    The latter two are somewhat confusing. Does that really

    mean that the the diameter of solder mask opening is smaller

    than the ball itself, ie, the copper should be partially

    covered from edges by the mask? (and follow up if so; "how

    that is done?")

     

     

    How is it done?

    Switch off the automatic generation of the solder stop symbols

    for your SMDs in the Package Editor (CHANGE STOP OFF) and draw

    the solder stop mask manually with a CRICLE. with = 0, in the

    tStop layer.

     

     

     

    Then, somehow I don't feel comfortable using very small (0.1mm)

    drills, but guess there is no way to avoid those? Or would it

    be better to use larger drill and smaller diameter copper

    around it?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm