EAGLE User Support (English) Not using Eagle Schematic Capture
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 244 views
  • Users 0 members are here
Related

Not using Eagle Schematic Capture

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I use Mentor Graphics Design Capture as my schematic entry package.  I am in

the process of finishing a ULP to import the netlist format to place parts

and import the nets (will probably finish today).

 

Do I have to create a schematic symbol in Eagle for each part in my library

even though I'm not using Eagle's schematic entry?

 

If this is the case, then this is a major short-coming of the software.

I've used probably 6 different PCB CAD packages and I've never seen anything

quite like the arrangement of your library database.  Quite frankly, the

hierarchy needs to be changed.

 

Thanks for any help.

 

Keith

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    On 2008/Apr/25 11:04 AM, in article fusrt6$7un$1@cheetah.cadsoft.de, "Klaus

    Schmidinger" <Klaus.Schmidinger@cadsoft.de> wrote:

     

    On 04/25/08 16:45, Keith wrote:

    Hi,

     

    I use Mentor Graphics Design Capture as my schematic entry package.  I

    am in the process of finishing a ULP to import the netlist format to

    place parts and import the nets (will probably finish today).

     

    Do I have to create a schematic symbol in Eagle for each part in my

    library even though I'm not using Eagle's schematic entry?

     

    If you're not useng EAGLE's schematic capture, then you don't

    have to create schematic symbols. You can use just the packages.

     

    Hello Keith,

     

    We have a tool to already import a PADS netlist into the EAGLE BRD editor.

    You can find it at www.eagletoolkit.com if you run into problems with your

    attempt.  There is a cost to it but it is also supported.  It doesn't take

    much debugging to make up the $100US cost of the tool.

     

    As part of that tool you can also export PADS netlist and PADS ECO file from

    EAGLE SCH editor.  But these may be of no use to you.

     

    If this is the case, then this is a major short-coming of the software.

    I've used probably 6 different PCB CAD packages and I've never seen

    anything quite like the arrangement of your library database.  Quite

    frankly, the hierarchy needs to be changed.

     

    Why would that be?

     

    I think think the point here, please correct me Keith if I'm off base, is

    that in order to add something to the schematic you have to have a device

    (symbol + footprint + mapping between them).  But strictly speaking, you

    only need the symbol (and not the footprint and mapping) to design a

    schematic.  So if you want to use EAGLE as the schematic editor only (and

    export the netlist as per the EET :: Pads Interface for instance) then you

    are actually forced to do some work that is really part of the PCB and will

    just be duplicated by the external PCB design file.

     

    Keith, one way around this, which is a bit of a kludge, is what we do

    internally.  Create a series of dummy packages that you can use for this

    very purpose.  Given you don't care about what the actual footprint looks

    like this works OK.  You still need to do the pin mapping but you'd need

    that anyways for the netlist.

     

    The downside is that all of the footprints have to be in the same library as

    all of the symbols.  This is another place where my suggestion to allow a

    device to use a footprint from an external library is of benefit--you don't

    have to have this list of dummy footprints in every library that you create.

     

    I hope this helps explain a bit Keith and perhaps allows you to use EAGLE in

    a bit more efficient way.

     

    James.

     

    --

    James Morrison

    www.eagletoolkit.com

    EAGLE Design Expert

    North American Online EAGLE Dealer

    EAGLE Enterprise Toolkit

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    On 2008/Apr/25 11:04 AM, in article fusrt6$7un$1@cheetah.cadsoft.de, "Klaus

    Schmidinger" <Klaus.Schmidinger@cadsoft.de> wrote:

     

    On 04/25/08 16:45, Keith wrote:

    Hi,

     

    I use Mentor Graphics Design Capture as my schematic entry package.  I

    am in the process of finishing a ULP to import the netlist format to

    place parts and import the nets (will probably finish today).

     

    Do I have to create a schematic symbol in Eagle for each part in my

    library even though I'm not using Eagle's schematic entry?

     

    If you're not useng EAGLE's schematic capture, then you don't

    have to create schematic symbols. You can use just the packages.

     

    Hello Keith,

     

    We have a tool to already import a PADS netlist into the EAGLE BRD editor.

    You can find it at www.eagletoolkit.com if you run into problems with your

    attempt.  There is a cost to it but it is also supported.  It doesn't take

    much debugging to make up the $100US cost of the tool.

     

    As part of that tool you can also export PADS netlist and PADS ECO file from

    EAGLE SCH editor.  But these may be of no use to you.

     

    If this is the case, then this is a major short-coming of the software.

    I've used probably 6 different PCB CAD packages and I've never seen

    anything quite like the arrangement of your library database.  Quite

    frankly, the hierarchy needs to be changed.

     

    Why would that be?

     

    I think think the point here, please correct me Keith if I'm off base, is

    that in order to add something to the schematic you have to have a device

    (symbol + footprint + mapping between them).  But strictly speaking, you

    only need the symbol (and not the footprint and mapping) to design a

    schematic.  So if you want to use EAGLE as the schematic editor only (and

    export the netlist as per the EET :: Pads Interface for instance) then you

    are actually forced to do some work that is really part of the PCB and will

    just be duplicated by the external PCB design file.

     

    Keith, one way around this, which is a bit of a kludge, is what we do

    internally.  Create a series of dummy packages that you can use for this

    very purpose.  Given you don't care about what the actual footprint looks

    like this works OK.  You still need to do the pin mapping but you'd need

    that anyways for the netlist.

     

    The downside is that all of the footprints have to be in the same library as

    all of the symbols.  This is another place where my suggestion to allow a

    device to use a footprint from an external library is of benefit--you don't

    have to have this list of dummy footprints in every library that you create.

     

    I hope this helps explain a bit Keith and perhaps allows you to use EAGLE in

    a bit more efficient way.

     

    James.

     

    --

    James Morrison

    www.eagletoolkit.com

    EAGLE Design Expert

    North American Online EAGLE Dealer

    EAGLE Enterprise Toolkit