EAGLE User Support (English) Autorouter: Some Traces (ex:+15V, +5V , -15V) thicker tracks routen
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
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 206 views
  • Users 0 members are here
Related

Autorouter: Some Traces (ex:+15V, +5V , -15V) thicker tracks routen

autodeskguest
autodeskguest over 17 years ago

 

I could not find a way in the autorouter to adjust some traces to be

thicker, For example: I want the supply traces to be a minimum of

20mils. Is it possible to do that.

 

thanks

FI

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    FI schrieb:

     

    I could not find a way in the autorouter to adjust some traces to be

    thicker, For example: I want the supply traces to be a minimum of

    20mils. Is it possible to do that.

     

    thanks

    FI

     

     

    Define nat classes and assign them to certain nets. The Autorouter

    will take them into consideration.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm