EAGLE User Support (English) Change width of all layed routes
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
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 300 views
  • Users 0 members are here
Related

Change width of all layed routes

autodeskguest
autodeskguest over 17 years ago

I am using the autorouter, but I am not happy with it's default thickness of

the routes.

 

Is there any way to change the thickness?

I was thinking perhaps there is a command like "change width 10 to 16" or

something like that.

 

Thanks!

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Kasper schrieb:

    I am using the autorouter, but I am not happy with it's default thickness of

    the routes.

     

    Is there any way to change the thickness?

    I was thinking perhaps there is a command like "change width 10 to 16" or

    something like that.

     

    Thanks!

     

     

     

    take a look at the post 'Autorouter: Some Traces (ex:+15V, +5V , -15V)

    thicker tracks routen' 28.04.2008 07:56

    or 'Autorouter', 18.04.2008 20:07

     

    you can create classes for your signals where you can set the thickness

    for each class

     

    just type: help class

    and you'll find the information you need

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Kasper schrieb:

    I am using the autorouter, but I am not happy with it's default thickness of

    the routes.

     

    Is there any way to change the thickness?

    I was thinking perhaps there is a command like "change width 10 to 16" or

    something like that.

     

    Thanks!

     

     

     

    take a look at the post 'Autorouter: Some Traces (ex:+15V, +5V , -15V)

    thicker tracks routen' 28.04.2008 07:56

    or 'Autorouter', 18.04.2008 20:07

     

    you can create classes for your signals where you can set the thickness

    for each class

     

    just type: help class

    and you'll find the information you need