Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) IC Design Across Hierarchical Blocks
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 771 views
  • Users 0 members are here
  • ic
  • optimization
  • alu
  • pcb layout
  • schemeatic
  • logic gate
Related

IC Design Across Hierarchical Blocks

jleazott
jleazott over 6 years ago

I am trying to make an 8 bit ALU in Eagle but I am running into a huge problem. I am using Eagle's module system to create an individual adder, then another to create a bit slice, lastly a few schematics to add all the extra components.

 

Here is the problem, each hierarchical block is purely independent of one another.

So each adder contains 2 XOR, 2 AND, and 1 OR gate. Since I am using the 74LS series (particularly the quad 2 input sets) I am only using half of the XOR, half the AND, and a quarter of the OR chip.

If I were to then place 2 adder modules in a schematic I would have 4 XOR, 4 AND, and 2 OR gates which works and ideally I would only use 3 IC's.

However, I instead end up with 6 because each adder instance uses 3.

I know with OrCAD this is fixed by Annotating and works really well and know there has to be something like this in Eagle.

I have tried using Eagles renumber parts but that does nothing for my situation.

 

I know I could use design blocks but I would prefer to keep the abstraction of no longer seeing what is inside the slice and also having it all update nicely when I change the module

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 6 years ago

    Jacob Leazott wrote:

     

    I am trying to make an 8 bit ALU in Eagle but I am running into a huge problem. I am using Eagle's module system to create an individual adder, then another to create a bit slice, lastly a few schematics to add all the extra components.

     

    Here is the problem, each hierarchical block is purely independent of one another.

    So each adder contains 2 XOR, 2 AND, and 1 OR gate. Since I am using the 74LS series (particularly the quad 2 input sets) I am only using half of the XOR, half the AND, and a quarter of the OR chip.

    If I were to then place 2 adder modules in a schematic I would have 4 XOR, 4 AND, and 2 OR gates which works and ideally I would only use 3 IC's.

    However, I instead end up with 6 because each adder instance uses 3.

    I know with OrCAD this is fixed by Annotating and works really well and know there has to be something like this in Eagle.

    I have tried using Eagles renumber parts but that does nothing for my situation.

     

    I know I could use design blocks but I would prefer to keep the abstraction of no longer seeing what is inside the slice and also having it all update nicely when I change the module

     

    Thanks

     

    Have you considered using 74..1G.. 74..2G.. ?

    May even make the layout easier.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 6 years ago

    Jacob Leazott wrote:

     

    I am trying to make an 8 bit ALU in Eagle but I am running into a huge problem. I am using Eagle's module system to create an individual adder, then another to create a bit slice, lastly a few schematics to add all the extra components.

     

    Here is the problem, each hierarchical block is purely independent of one another.

    So each adder contains 2 XOR, 2 AND, and 1 OR gate. Since I am using the 74LS series (particularly the quad 2 input sets) I am only using half of the XOR, half the AND, and a quarter of the OR chip.

    If I were to then place 2 adder modules in a schematic I would have 4 XOR, 4 AND, and 2 OR gates which works and ideally I would only use 3 IC's.

    However, I instead end up with 6 because each adder instance uses 3.

    I know with OrCAD this is fixed by Annotating and works really well and know there has to be something like this in Eagle.

    I have tried using Eagles renumber parts but that does nothing for my situation.

     

    I know I could use design blocks but I would prefer to keep the abstraction of no longer seeing what is inside the slice and also having it all update nicely when I change the module

     

    Thanks

     

    Have you considered using 74..1G.. 74..2G.. ?

    May even make the layout easier.

    --

     

    Lorenz