Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Streaky/split polygon ground plane
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 187 subscribers
  • Views 576 views
  • Users 0 members are here
Related

Streaky/split polygon ground plane

autodeskguest
autodeskguest over 18 years ago

Searching the newsgroup for an answer to this one didn't turn up any

matches (but I think I know a lot more about ground planes/polygons now!).

 

I have designed a double-sided board with ground planes on both sides

of the board.  When I print (as in File->print) the board with output

to a Postscript file, then view it (using evince - I'm running Ubuntu

by the way), I see both the top and bottom ground planes have small

horizontal slits in them.  A photo is worth 1000 words as they say.

 

Notice that the edge of the polygon is never affected, just the

inside.  Other signals (the regular looking traces in the image)

appear just fine as well.  The width of the polygon affects the

spacing of the streaking.  It's like there isn't any overlap of the

lines used to create the solid fill, and sometimes we see 'through'

between the lines.

 

I have also tried printing to a 'PDF printer' - a driver that acts

like a printer to the app, but redirects output to a file in PDF

format.  Using xpdf to view that file also shows the streaking effect.

 

This doesn't seem to affect the CAM files.  I have viewed those using

ViewMate without any streaking apparent.

 

All this has arisen because I wish to send a PDF of my layout to

someone for checking.  They don't run Eagle so I need some image

format that they can read.  I suspect I'll get a ribbing from them for

not running Protel; grr!

 

Any ideas how to stop this odd phenomenon would be appreciated.

 

Photo attached (hopefully).

 

-Martin

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • eur
    eur over 18 years ago

    On 2008-05-08 07:45:39 +0200, Martin van den Nieuwelaar

    <martin@rawl.co.nz> said:

     

    I have designed a double-sided board with ground planes on both sides

    of the board.  When I print (as in File->print) the board with output

    to a Postscript file, then view it (using evince - I'm running Ubuntu

    by the way), I see both the top and bottom ground planes have small

    horizontal slits in them.  A photo is worth 1000 words as they say.

     

    The photo came through OK.

     

    You have a lot of layers turned on. If you display only the top layer,

    do you still see the slits?

     

    I suspect this is a graphics problem of your OS, not Eagle.

     

     

    Notice that the edge of the polygon is never affected, just the

    inside.  Other signals (the regular looking traces in the image)

    appear just fine as well.  The width of the polygon affects the

    spacing of the streaking.  It's like there isn't any overlap of the

    lines used to create the solid fill, and sometimes we see 'through'

    between the lines.

     

    You could try to change -> pour -> hatched and then back to fill, does 

    that help?

     

     

     

    --

    Eur van Andel  eur@fiwihex.nl

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • eur
    eur over 18 years ago

    On 2008-05-08 07:45:39 +0200, Martin van den Nieuwelaar

    <martin@rawl.co.nz> said:

     

    I have designed a double-sided board with ground planes on both sides

    of the board.  When I print (as in File->print) the board with output

    to a Postscript file, then view it (using evince - I'm running Ubuntu

    by the way), I see both the top and bottom ground planes have small

    horizontal slits in them.  A photo is worth 1000 words as they say.

     

    The photo came through OK.

     

    You have a lot of layers turned on. If you display only the top layer,

    do you still see the slits?

     

    I suspect this is a graphics problem of your OS, not Eagle.

     

     

    Notice that the edge of the polygon is never affected, just the

    inside.  Other signals (the regular looking traces in the image)

    appear just fine as well.  The width of the polygon affects the

    spacing of the streaking.  It's like there isn't any overlap of the

    lines used to create the solid fill, and sometimes we see 'through'

    between the lines.

     

    You could try to change -> pour -> hatched and then back to fill, does 

    that help?

     

     

     

    --

    Eur van Andel  eur@fiwihex.nl

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data